text.skipToContent text.skipToNavigation

Legrand Launches P500 Player Portfolio Sound Bar

Software Update For Sound Bar Support Now Available; Company Opens Ordering



Hebron, Kentucky
March 30, 2017
 

Legrand, the global specialist in electrical and digital building infrastructures, announced it has launched the Nuvo P500 Player Portfolio sound bar, including the immediate availability of the software update, Version 4.1.2, required to use the new sound bar-subwoofer combo as part of the Player Portfolio home music system. The company said it has also begun accepting dealer orders for the P500, with deliveries starting in April.

Current Player Portfolio owners will automatically be notified that the 4.1.2 software is available for download from the Legrand website.

The P500 Sound Bar’s powerful 2.1 speaker system provides enhanced audio for TV and movies while doubling as a Nuvo Player for music and other audio streaming content via online services, home networks, or personal iOS or Android devices. The Player Portfolio supports Spotify, Pandora, iHeartRadio, Deezer, Sirius XM and other popular streaming services. 

“The P500 is an important piece in the evolution of our Player Portfolio line,” said Desirée Webster, Senior Marketing Communications Manager. “There has been a lot of anticipation building up to this point for us and our dealers. Our goal is to provide flexible home audio solutions for professional installersand this new double-duty Player drives that point home.” 

The P500’s eight-inch wireless subwoofer delivers deep, clean low-frequency response. All listening experiences are customizable with four audio modes—movie, music, voice and night mode.


​​​​​​​A Great Looking System with Many Control Options

A sleek industrial design, with a metal grill, white backlit touch panel and a neatly hidden internal power supply make the P500 ideal for installation below flat panel TVs and an attractive addition to any room in the home.

The innovative system provides easy and flexible control options, including its own remote control, the Nuvo Player app and optional in-wall keypads. As part of the Nuvo Player Portfolio, it has integrated control via drivers for Control4, Crestron, RTI, URC and KNX. The unit also features a built-in IR learning function, which enables control via third-party remotes sold with TVs and set top boxes.

The P500 can be installed in either an Ethernet or wireless (802.11 a.b.g.n. 2.4GHz or 5.1GHz) configuration and additional components can be connected to it via TOSLINK and analog line inputs.

The Nuvo P500 will be available in April for MSRP $899.

Please click here for P500 sound bar and subwoofer images.


About Legrand

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.3 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819) www.legrand.us

#  #  #

 

  

Media Contacts:

Feintuch Communications
Doug Wright / Richard Roher                                                 
212-808-4903 / 917-207-9604
legrand@feintuchpr.com