text.skipToContent text.skipToNavigation

At Ise, Legrand Features Nuvo P4300, New Multi-zone, Rack-mount Player For Player Portfolio Music System

Features Simplified Setup and Diagnostics Via Touch Screen Display and Delivers Highest Quality Audio to Three Zones Simultaneously with 110-Watts of Power

 

Amsterdam
February 7, 2017
 

​​​​​​​Legrand, the global specialist in electrical and digital building infrastructures, showcases its Nuvo P4300 Player, the newest rack-mount model to its Player Portfolio line at ISE 2017. The model is the most powerful, efficient unit yet and boasts simplified installation and diagnostics for installations with a backlit touch screen display. Designed by audiophiles for installation by professionals, the three source, three amplifier design enables three independent sources of audio content to be played in three rooms simultaneously.

The P4300 allow users to get even more enjoyment from their favorite music from popular streaming services, including Spotify, iHeartRadio, TuneIn, Napster, Deezer and SiriusXM, as well as from content stored on networked computers and iOS and Android portable devices. Super efficient Class D amplifiers deliver the highest quality audio with 110 Watts of power that remains consistent when set to 4, 6 or 8 ohm within the app during setup.

“The P4300 hands down delivers the best professional whole home audio system yet. It pairs the experience of the users’ music, when and where they want it, with incredible power and clarity,” said Walt Zerbe, Legrand’s product manager for audio. “The model is very strong from an installation standpoint, offering a rack-mount solution that packs multiple amps in a single space, a cooler running unit and the added value of the backlit touch screen for gauging diagnostics. It’s the right product for the professional integrator and ultimately delivers the experience the customer is looking for.”

The model’s backlit touch screen display shows system status and zone name in addition to system configuration information that aids in installation. All line inputs and line outputs use a combination 3.5mm analog/Toslink connection. Plus, the unit’s side-mounted heat sinks allow convenient single-space rack mounting to conserve space and increase installation flexibility in the rack.

The Nuvo P4300 is currently available for MSRP $2,299.00.

For more information on the model, please click here.

About Legrand

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.3 billion in 2015. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819) www.legrand.us

#  #  #

 

Media Contacts:

Feintuch Communications
Doug Wright / Richard Roher                                                 
212-808-4903 / 917-207-9604
legrand@feintuchpr.com