text.skipToContent text.skipToNavigation

New Legrand Active Optical HDMI Cables Deliver 4K, Ultra HD and HDR Content Over Distances up to 75 Meters


These 18Gbps AOC HDMI Cables, available in lengths of 10 meters (32.8 feet; Model AC2F10-BK), 20 meters (65.6 feet; Model AC2F20-BK), 50 meters (164 feet; Model AC2F50-BK) and 75 meters (246.1 feet; Model AC2F75-BK), distribute content with 100 percent reliability and no signal loss or dropouts.


​​​​​​​HEBRON, Ky., June 26, 2017 – Legrand, the global specialist in electrical and digital building infrastructures, unveils four new Active Optical (AOC) HDMI cables that can distribute high-definition HDMI signals, including 4K UltraHD and HDR content, and other high-speed, high-performance AV features, to distances of up to 75 meters (246 feet).

These 18Gbps AOC HDMI Cables, available in lengths of 10 meters (32.8 feet; Model AC2F10-BK), 20 meters (65.6 feet; Model AC2F20-BK), 50 meters (164 feet; Model AC2F50-BK) and 75 meters (246.1 feet; Model AC2F75-BK), distribute content with 100 percent reliability and no signal loss or dropouts. Ideal for light commercial and residential projects, the cables are constructed with plastic optical fiber, allowing optimum performance at extended distances and added flexibility for easy installation in tight spaces. 

Self-powered by the source device to which they are connected, these cables eliminate the need for external power adapters. The HDMI connection ends are also color-coded to ensure correct directional installation and offer an enhanced grip to provide the most secure connection points. The new cables are CMP Plenum rated, which covers both CMG and CL2-3 for in-wall use in commercial and residential installations.

“We regularly hear from our customers that new video standards challenge them to find cables that will reliably deliver higher resolution content over extended distances,” said Fritz Werder, Legrand VP and general manager, On-Q and Nuvo lines. “These cables effectively future-proof residential and light commercial spaces for new technologies, while offering more flexibility and options for monitor placement, as well as fewer points of failure versus traditional signal extender products. They will solve a lot of problems for installers.”

The cables have been third-party tested to ensure their ability to handle the full 18Gbps data speeds necessary to deliver today’s 4K/UHD 60Hz video resolution, which delivers four times the picture density and noticeably clearer images than the 1080p high-definition standard. Products equipped to play or display vibrant, color-rich HDR content require cables that can deliver high-speed, high-bandwidth performance.

For additional information about Legrand’s AOC HDMI cables, click here. 

About Legrand and Legrand, North & Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $5.6 billion in 2016. Legrand has a strong presence in North and Central America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, QMotion, Quiktron, Raritan, Solarfective, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819) www.legrand.us. 


​​​​​​​Media Contacts:

Feintuch Communications

Doug Wright / Richard Roher

212-808-4903 / 917-207-9604  legrand@feintuchpr.com