VIEW All news   |   Cablofil   |   On-Q   |   Ortronics   |   Pass & Seymour   |   Wiremold   |   adorne   |   Archive RSS

Mohegan Sun Installs Electric Vehicle Chargers From Legrand

SYRACUSE, NY, November 19, 2012 – The Mohegan Sun has installed two of Legrand’s Level 2 Wall-mounted Electric Vehicle Charging Stations (EV Chargers) at their Connecticut-based resort as a service to guests and patrons. As the demand for charging facilities grows, the Mohegan Sun is expected to install several more chargers.

Owned by the Mohegan Tribe, the busy Mohegan Sun draws 25,000 daily visitors to its three casinos, more than 65 dining and premium retail outlets and finest entertainment at three world-class venues. The Mohegan Sun boasts a 1,200-room luxury hotel with 100,000 square feet of premier meeting space as well as a luxurious spa.

Commenting on the installation of the EV Chargers, Michael Hamilton, Vice President of Resort Operations at the Mohegan Sun said, “We installed Legrand’s Electric Vehicle Chargers for a number of reasons. We are a customer centric organization and we wanted to ensure that guests who drive electric vehicles have access to this important service. It is also important for us to show our customers that we are an environmentally conscious organization and that we support their sustainability values. Ultimately, the market for electric vehicles is set to increase and it is important to have an electric vehicle charging system in place meet the anticipated demands of our guests.”

The EV Chargers were installed in Mohegan Sun’s underground parking garage on the B1 level, close to the entry and exit ramps used by the resort’s valet service. This also provides easy access for the transportation department, who will receive the electric vehicle from the valets and handle the responsibility of parking and charging guest’s electric vehicles.

The installation of the Level 2 Chargers was a seamless process for the Mohegan Sun. The charging stations were situated close to an electrical distribution room so a minimal amount of materials, such as conduits, fittings and wire were used. This also helped ensure that installation costs were kept as low as possible. “Mounting the charging units was straight forward and the instructions with the units were easy to comprehend and follow,” added Hamilton.

The EV Chargers were mounted in such a way that the transportation department could take advantage of their long charging cords and power up four vehicles, parked two deep, from one charging unit. In total, eight vehicles can be charged at one time without moving any vehicle after parking them in a designated parking place.

“Ease of installation and use coupled with reliability and the ability to rapidly charge electric vehicles are critical factors in deciding what Electric Vehicle Charger to select, particularly for light commercial applications,” said Kiran Laxman, product manager of electric vehicle supply equipment at Legrand/Pass & Seymour.

Mohegan Sun has several hybrid vehicles in its fleet that are used by a number of different departments throughout its extensive property. It is currently investigating purchasing electric vehicles at a later date.

- Legrand Level 2 Chargers for Residential and Commercial Applications–

Legrand’s Level 2 chargers are perfectly suited for both residential and light commercial applications and are hard-wired to a 20A circuit. They charge vehicles faster – approximately three to six hours. The Level 2 20A/240V chargers are also weatherproof rated and have built-in ground fault protection.

Legrand also offers a Level 2 Pedestal-Mounted EV Charging Station that is ETL-certified and is available in both single and dual configurations, making it perfect for installation at light commercial sites such as hotels and resorts, office parks, apartment complexes and shopping malls.

The 20A/240V EV Charging Station is fixed on a sturdy, anodized aluminum Vista Architectural™ column that provides support for both the single and dual charging station configurations. It is also fully weatherproof with a NEMA 3R rating and can be installed outdoors or indoors in covered parking/charging areas.

For busy users who want to charge their electric vehicles on the road, Legrand also has a Level 1 15A/120V charger. It is weatherproof for indoor or outdoor use, plugs into a standard 15A or 20A receptacle and includes built-in ground fault protection.


# # #


Connect with Legrand/Pass & Seymour on Facebook www.facebook.com/legrandna, Twitter www.twitter.com/passandseymour or www.twitter.com/legrandna, and YouTube www.youtube.com/legrandna

 

# # #


 

About Legrand

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of $5.8 billion in 2011.  Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819). www.legrand.us

 

About Mohegan Sun

Mohegan Sun, owned by the Mohegan Tribal Gaming Authority, is one of the largest, most distinctive and spectacular entertainment, gaming, shopping and dining destinations in the United States. Situated on 185 acres along the Thames River in scenic southeastern Connecticut, Mohegan Sun is within easy access of New York, Boston, Hartford and Providence and located 15 minutes from the museums, antique shops and waterfront of Mystic Country. More information is available by calling 1.888.226.7711 or visiting mohegansun.com . Connect with us on facebook.com/mohegansun , follow us on twitter.com/mohegansun and view us on youtube.com/mohegansunvideos .

 

 

CONTACT

 

Evan Bloom

(315) 413-4349
ebloom@mower.com

 

 
Close website feedback

1. Thanks for visiting Legrand. How would you rate your overall experience with the Legrand website today?











1 = Poor 10 = Excellent
2. Which best describes you?
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
(5) How critical to your projects or business are Legrand products?