VIEW All news   |   Cablofil   |   On-Q   |   Ortronics   |   Pass & Seymour   |   Wiremold   |   Archive RSS

Versatile Round Floor Box for Raised Floor and Wood Floor Applications

WEST HARTFORD, Conn., January 21, 2011 – A recessed round floor box from Legrand/Wiremold provides a high level of functionality and flexibility in raised and wood floor applications. The Wiremold® CRFB Series floor box fits into a standard raised floor air diffuser opening, providing easy access to recessed devices. This floor box is also approved for use in wood floors, including elevated platforms, stages, and balconies.

The CRFB Series floor box features four separate compartments that can accommodate multiple combinations of power, communication, and audio/video services. A tunnel feature allows two of the compartments to be used for a single service, while the other two are used for different services. Thus, these boxes can be field configured or reconfigured to accommodate power only, communication only, audio/video only, or combinations in a single unit. Trade size 1/2", 3/4", 1-1/4", and 2" knockouts accommodate standard conduit.

Standard CRFB covers offer large wire/cable egress with a locking feature. These floor boxes also accept round 8" Evolution Series poke-thru covers. This increases the ability to match aesthetics throughout the building. Die-cast aluminum covers are available in black, gray, nickel, brass, and bronze painted finishes.

CRFB Series floor boxes are listed by Underwriters Laboratories Inc. to U.S. and Canadian safety standards for raised floors and wood floors. They meet NEC Section 300-22 and are suitable for use in air handling spaces and raised floor plenums. They are manufactured in the United States and comply with all BAA (Buy American Act) and NAFTA (North American Free Trade Act) requirements.


About Legrand/Wiremold
Legrand/Wiremold, headquartered in West Hartford, Conn., is the leader in wire and cable management systems, including metal and nonmetallic raceways, power-poles, poke-thru devices, floor boxes, Walker® underfloor systems, plug-in outlet centers, firestopping systems, and innovative architectural columns. Please visit http://www.legrand.us/Wiremold.aspx or call 1-800-621-0049.

About Legrand
Legrand is the global specialist in products and systems for electrical installations and information networks where people live and work. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for suppliers worldwide. Legrand has a strong presence in the North American market, with a portfolio of products that includes Cablofil, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is actively expanding its market divisions that include Electrical Wiring Systems, Home Systems, Lighting Controls and Commercial Datacom. Innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $5.0 billion in 2009. The company is listed on Euronext and is a component stock of indexes including the SBF120. FTSE4Good, MSCI World and ASPI (ISIN code FR0010307819). www.legrand.us

###