News: Legrand Acquires AFCO Systems Cabinet & Containment Solutions
Industry leader in the design, engineering and manufacturing of products for the data center, collocation and telecommunications industries.
Menu
Search
Menu

Router Compatibility List

* = WiFi Alliance Certified

Hardware Make Model(s) Compatible/Tested Works out of the box Known Issues
Router/Switch Arris TG862G-CT*
SBG-6580*
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module No Under the Advanced Options menu - the "Multicast Enable" option must be enabled.
Router/Switch Actiontec (Verizon) MI424WR* Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module Yes
Router/Switch Legrand DA2154-V1
DA1054
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module, Intuity Yes
Router/Switch D-LINK DIR-865L (v1.03 and v1.06)*
DIR-655 (v3.00 and 3.02)*
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module, Intuity No DIR865L - Firmware v1.03 - IPV4 Multicast Streaming is not enabled by default. This option will need to be checked. This issue is corrected in v1.06 firmware.
DIR-655 - Firmware 3.00 - Firmware v1.03 - IPV4 Multicast Streaming is not enabled by default. This option will need to be checked. This issue is corrected in v1.06 firmware.
Router/Switch TP-LINK Archer C7 V2* (v.131217 and v.150304)
TP-WR841N* (v3.14.4 and 3.16.9)
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module, Intuity No For the Archer C7 v131217, IGMP Proxy will need to be disabled under the Network>IPTV menu selection.
Router/Switch Buffalo WZR-600DHP* (v20180 and v245PZ)
WCR-GN* (v1.04 and v1.08)
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module, Intuity Yes None
Router/Switch Motorola NVG-589 Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module, Intuity Yes
Router/Switch LuXul
XWR-1750
XWR-1200
XWR-3100
ABR-4400
XBR-4400
ABR-4500
XBR-4500
ABR-5000
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module Yes None
Router/Switch Cisco / Linksys EA4500*
EA6500*
E2500*
WRT-54GL* (v4.30.14 and v4.30.16)
E1200* (v2.0.04 and 2.0.07)
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module , Intuity (WRT-54GL, E1200) Yes None
Router/Switch Netgear Nighthawk R7000 WNDRMACV2
WNDR3700v4*
(v1.0.1.42 and 1.0.2.78)
WNDR4300v2* (1.0.0.26)
WNR100v3*
ADSL Modem Model 7550
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module, Intuity Yes None
Router/Switch Technicolor TC-8305*
C2000T (Century Link)*
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module, Intuity (C2000T) Yes None
Router/Switch ASUS RT-N56U* (v.3.0.0.4374_4561)
RT-N53* (v3.0.0.4.374_311 and v3.0.0.4.376.3754)
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module, Intuity Yes None
Access Points Legrand DA1101
DA1104
Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module, Intuity Yes
Access Points LuXul XAP-1230

XAP-1510

XAP-1410

XAP-1210

XAP-310

XWO-BAP1

XAP-1240

Nuvo Player Portfolio, On-Q Digital Audio, On-Q lyriQ Digital Streaming Module Yes None

Incompatible Devices

Except DPC3825 and DPC3939SC101T Netgear
Hardware Make Model Issue Remedy
Router/ Switch Actiontec GT724WGR
M1000
C1000A
1000
PK5000
These model routers/modems do not fully support the passing of multicast packets via the wired and wireless networks. A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ Switch Alcatel Lucent I-240W-R
I-240W-Q
I-240W-T
These model routers/modems do not allow multicast packets to pass between the wired and wireless connections on the router/modem. A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/Switch TrendNet TEW-812-DRU (v2.0.10.0) These model routers/modems do not fully support the passing of multicast packets via the wired and wireless networks. The Intuity system does not commission properly when using this router device. A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ Switch Belkin F7D4301
F7D4302
F7Dxxxx
These model routers/modems do not fully support the passing of multicast packets via the wired and wireless networks. A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ Switch Belkin F9K1103 This router does not support the passing of proper IGMP packets. Some functions of the On-Q system may not work properly. A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ Switch Cisco All DPC/EPC/DPQ models
These model routers/modems do not fully support the passing of multicast packets to the SSDP destination port (UDP Port 1900). A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ Switch Huawei HG532d These model routers/modems do not fully support the passing of multicast packets to the SSDP destination port (UDP Port 1900). A Legrand or third party wireless access point is needed. We recommend the DA2154-V1.
Router/ Switch KPN InternetPlus Modem This router blocks all UPnP traffic. An additional router will be necessary between this device and the On-Q or NuVo audio system.
Router/ Switch Linksys WCG200-C Comcast provided device. This device only supports 5 local IP addresses. There is no way to increase the local DHCP IP address pool.
Router/ Switch Netgear CG814WGv1
CG814WGv2
Comcast provided device. This device only supports 4 local IP addresses. The locsal DHCP pool can be increased but only 4 local devices will have internet access.
Router/Switch Netgear R6250 Does not properly support mDSN discovery. None.
Router/Switch Ubee DDW3201B This model routers/modems do not allow multicast packets to pass between the wired and wireless connections on the router/modem by default. Enable "Multicast Enable" in the router settings.
Router/Switch Ubee DDW365 This model routers/modems do not allow multicast packets to pass between the wired and wireless connections on the router/modem by default. Enable "Multicast Enable" in the router settings.
Router/ Switch US Robotics USR 8054 These model routers/modems do not fully support the passing of multicast packets via the wired and wireless networks. Enable 'Multicast Streaming' in the router settings.
NAS Drives Fantec All Models No support for Windows File Sharing (SMB). None.
NAS Drives Hawking HNAS1 Defaults to static IP of 192.168.1.1. This creates an IP conflict with a large number of routers. Use the setup CD to assign an IP address outside of the DHCP scope.
NAS Drives Level One FNS 1000 Built-in DHCP server is enabled by default. Can create IP address conflicts. Also defaults to a static IP address. Disable DHCP server and give the NAS a static IP.
NAS Drives Netgear SC101
This device is an NDAS, it requires the computer to be on and running software in order to access the files stored on it. None.