NEWS: Legrand acquires Focal Point
A Chicago-based, vertically integrated leader in architectural lighting and acoustic solutions.
Menu
Search
Menu
RSS Feed

Legrand Introduces Infinium Quantum™

New end-to-end fiber system provides the industry’s lowest loss optical cabling solution for high-speed and high-bandwidth applications


West Hartford, CT – January 20,2020 Today Legrand North and Central America (LNCA), a global innovation leader in power, light, and data technologies for homes, workplaces, and data centers, introduced Infinium Quantum™ -- the industry’s lowest loss optical fiber system designed for advanced data center applications.  Available in both single-mode and multimode, the patent pending Infinium Quantum systems offer the lowest channel link loss at 0.75dB, which is a recorded 64% improvement over standard systems and a 38% improvement over any ultra low-loss optical fiber system available on the market. 

Infinium Quantum, which becomes Legrand’s premium optical fiber system, was exclusively designed to allow the fastest and most reliable migration path to 400G and beyond by reducing or eliminating the need to replace cabling components. The Infinium Quantum system can be configured in 8-, 12- or 24-fiber connectivity for all Ethernet system options utilizing Base-8 or Base-12, depending on the specific IEEE 802.3 standard for 100Gb/s, 200Gb/s or 400Gb/s transmission.

Reliability of any optical fiber system is dependent on the link loss budget, which combines the total of connector loss with the cable loss. The loss budget has two uses: 1) during the design stage to ensure the cabling plant will work with the links intended to be used over it; and, 2) after installation, the loss budget is compared to the calculated loss to test results to ensure the cable plant is installed properly. “With higher speeds and higher bandwidths, the total link loss budget tolerances are becoming tighter and the overall component losses are becoming smaller. Understanding the relationship between total component loss and its effects on the entire network performance allows a system designer to implement a reliable cabling infrastructure for current and future needs and provides flexibility to support new technologies and architectures by simply updating the transceivers,” explains Randy Harris, Senior Product Manager at Legrand. “The Infinium Quantum system is based on a combination of superior engineering and unique patent-pending manufacturing processes of each of the connectivity components, which include high-density enclosures and panels, cassettes, trunk cable assemblies and patch cords,” he adds. 

TIA-568.3-D standard allows a multimode connector loss to a maximum of 0.75dB each. However, typical multimode connectors have losses of 0.2-0.5dB; factory-made and fusion-spliced single-mode connectors have losses of 0.1-0.2dB; and field terminated single-mode connectors have losses ranging from 0.5-1.0dB. “Introducing a fiber system with a loss of four connections for a combined total channel loss of .75dB is revolutionary in our industry and this becomes increasingly critical for evolving data centers, such as hyperscale environments,” Harris further explains. Any additional loss will depend on the specific fiber type and link distance.

In addition, the Infinium Quantum provides additional energy savings – up to 30% — based on the transceiver power consumption. A key factor in the lower loss and energy savings is the design of angled multimode connectivity for high-bandwidth transceiver transmission.  “Typically single-mode systems employ angled connectors but with today’s VCSEL transceivers, which are required for high-bandwidth multimode systems, these generate more heat, which can create additional back reflections.  Therefore, the multimode angled solution ultimately provides better optical return loss performance,” describes Harris. The Infinium Quantum’s single-mode total channel connection return loss is -55dB and the multimode system return loss is -34dB. “Some of the high-end transceivers are tunable at the output level and if there is a better performing system the power can be turned down, which directly correlates with electricity savings, making the Infinium Quantum system more sustainable too,” he concludes.

Pricing and Availability

For pricing, lead time, and availability through our distribution partners, please contact your local Legrand sales representative.

To learn more about the Infinium Quantum™, please visit www.legrand.us/infiniumquantum

###

 

About Legrand and Legrand, North and Central America

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Drawing on an approach that involves all teams and stakeholders, Legrand is pursuing its strategy of profitable and sustainable growth driven by acquisitions and innovation, with a steady flow of new offerings—including connected products stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand is one of the most sustainable companies in the world, as ranked by the Corporate Knights, and is committed to achieving carbon, water, and waste reductions in its operations, deepening its community relationships, and continuously improving the environmental profile of its products. Legrand reported sales of around $7.1 billion (USD) in 2018. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, www.legrand.us.

###

Media Contact:

Rosa Allyn

Marketing Communications

Rosa.Allyn@legrand.us