COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Nuvo Adds In-Wall Keypad Control to Player Portfolio Whole-Home Audio System


DALLAS, October 15, 2015 Legrand has announced two new additions to its Nuvo Player Portfolio hybrid audio system here at the 2015 CEDIA Expo that are focused at giving installers more flexibility for meeting customer needs. The new Nuvo P10 Keypad, a wall-mounted, Power-over-Ethernet keypad that delivers single-zone control of the audio’s volume, track, and source, makes the Player Portfolio the first wired/wireless system to offer an integrated keypad option. The company also announced new drivers for Crestron and Control4 that deliver seamless integration of the Player Portfolio homes using these popular control systems.

“Both the P10 Keypad and the new drivers are representative of our ongoing commitment to our dealers and providing the support they need to highlight the unique features of the Nuvo Player Portfolio,” said Fritz Werder, VP and general manager of Legrand’s On-Q and Nuvo lines. “The P10 provides the simple, architectural control point not found on other multi-room wireless audio systems, and the new drivers add enhanced compatibility with two of the most popular control software platforms.”

The P10 works in perfect sync with Nuvo’s Player App found on phones and tablets, and it offers quick access to the system’s basic functions, including volume/mute, play/pause, next/previous track navigation, as well as a “Favorites” button that allows the user to quickly scroll through up to five of their preset favorites at the preferred volume.

Incorporating PoE technology to simplify installation, the single-gang P10 uses only a single, powered Cat5 cable to power and control the system’s functions in the local zone. And with three available colors (white, light almond, and nickel), it is versatile to the décor. The P10 will be available to ship in November.

Crestron and Control 4 drivers can be downloaded now from Legrand’s website as well as through Crestron and Control 4.

For more information, call 800-223-4162 or visit www.legrand.us

#  #  #


Link to Images:

P10 Keypad 1

P10 Keypad 2

Media Contact:

Roher Public Relations

Torin Roher

971-266-8870 / 212-808-4904

legrand@roherpr.com