COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

On-Q/Legrand Unveils the Revolutionary Studio Collection


Harrisburg, PA, September 4, 2008 - On-Q/Legrand, the leader in home systems, announced today that at CEDIA it will reveal the complete Studio Collection, a series of products inspired by color and design trends from around the world. The Studio Collection embodies both elegant design and advanced functionality, and includes intercom, audio and camera systems.

"The Studio Collection represents On-Q's vision of the future of home technology; products that are intuitive in operation, comprehensive in functionality and contemporary in design," said Dan Tarkoff, vice president of product management and engineering at On-Q/Legrand. "No longer are plates and devices on the wall a visual afterthought. These products are creating an entirely new conversation around home decor in an area where homeowners historically had little to no options."

The Studio Collection includes:

  • The Selective Call Intercom System: This revolutionary intercom system features innovative technology, unmatched personalization, and easy, one-person installation. It enables room-to-room communication at the touch of a button, and supports up to three simultaneous, private conversations - the only intercom in the industry to do so.
  • The lyriQ Whole House Audio System: Available in both multi-source and single source versions, the lyriQ system distributes high quality audio throughout the home and even outdoors. One room or the whole house can be controlled from each keypad or through use of a universal remote. The system also includes a local source input, allowing music from a local source such as an iPod to override the main source music in one room.
  • The On-Q Camera System: This camera system includes a new, unobtrusive ball camera with no external wires or mounts. The camera installs easily in a single gang opening, and enables color video with optional audio. It's also optimized for low light conditions and features a weatherproof finish, enabling easy outdoor monitoring at any time of day. The system also includes two options for viewing camera images - a new LCD Console, equipped with a 7" screen to provide wide-angle viewing, and a TV Display Interface, which enables viewing of camera images on the TV screen.
  • 1-, 2-, 3-, or 4-Gang Wall Plates: Available in 17 contemporary color options, these decorator style plates feature a design and form-factor never before available to homeowners. The design, a sculptural flow of curves with titanium edging and a screwless finish, offers customers a new way to integrate home systems products with personal style and taste throughout the entire home.

Visit On-Q's booth, #214, at CEDIA to experience the inspired look of the Studio Collection and view demonstrations of each of the Studio Collection devices.

About On-Q/Legrand

By combining an innovative lifestyle-solutions approach to selling home technology with elegant, award-winning products, On-Q/Legrand is the only source you need to succeed in the home systems market. Headquartered in Harrisburg, Pa., On-Q/Legrand manufactures home technology products which are sold and installed through a network of distributors, dealers and residential builders. Learn more about us on the web at www.onqlegrand.com.

###