COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand Announces New Outdoor Wireless Access Point

Weatherproof WAP Features Functionality of Best Indoor Options, Extending The Home Network To The Pool, Patio, And Beyond


INDIANAPOLIS, IN, September 4, 2012 – Legrand, the leader in home technologies and solutions, announces the release of a new Outdoor 802.11n Wireless Access Point (WAP). The Outdoor WAP joins an existing family of LAN, indoor wireless, MoCA and powerline solutions designed specifically to give custom installers a complete, versatile set of home networking tools that meet the current and future needs of the connected household.

“Outdoor entertainment is such an important part of so many of our customers’ lifestyles,” said Fritz Werder, vice president and general manager for Legrand's Home Systems division. “But until now, the wireless networks that are an integral component of outdoor entertainment have resided indoors. Our new Outdoor WAP breaks down the barriers that have kept the network captive and extends the streaming, surfing, and control experience throughout our customers’ properties.” 

The Outdoor 802.11n Wireless Access Point boasts all of the latest connectivity and security options that are expected from a high-quality WAP, including 64/128-bit WEP, WPA / WPA2, WPA-PSK / WPA2-PSK and 802.1x authority to secure and protect a wireless LAN; MAC filtering and SSID broadcast control; static or dynamic IP addressing. It also features three modes of operation: Bridge, Gateway, and Wireless ISP Mode, and comes with a handy Setup Wizard to make configuration a snap.

To protect it from the elements, the Outdoor 802.11n WAP features a weatherproof IP-55 enclosure. Included in the package is a power over Cat 5 injector and AC power adapter (which much be installed indoors) to remote power the WAP, which can be conveniently installed indoors or outdoors. The WAP is designed to be easily pole-mounted (with two included mounting ties) or affixed to a flat surface for the utmost in installation flexibility.

Legrand’s Outdoor 802.11n Wireless Access Point will be available in November.
 
For additional information, visit www.legrand.us/onq

About Legrand

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $5.7 billion in 2010. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. www.legrand.us.