COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Desktop Networking Products from Legrand Expands Retrofit Options for Wired and Wireless Home Networks

Easy-to-install devices with latest technologies ensure a fast, reliable connection throughout the home.


Desktop Networking Press Release

HARRISBURG, Pa., July 18, 2013 – Legrand, the leader in connected home systems, today announced the release of four desktop networking products designed to ensure fast, reliable network connections throughout the home.

“At Legrand, we strive to deliver the best solutions when it comes to home networking,” said Fritz Werder, VP and General Manager, Legrand Home Systems Division. “These new desktop networking products expand our easy to install, retrofit home networking options.”

5-Port and 8-Port Gigabit Ethernet Switches

The new Desktop 5-Port (DA1015-V1) and 8-Port (DA1018-V1) Gigabit Ethernet Switches provide high performance, low cost options to upgrade or expand an older network to the networked TV, gaming system, and other bandwidth demanding devices at Gigabit speeds (1000Mbps).   As part of a complete Gigabit home network, all networked devices can have access to the fastest, highest quality connections.

802.11n Wireless Router

The Desktop 802.11n Wireless Router (DA2154-V1) provides broad, reliable Wi-Fi coverage throughout the home at speeds up to 300Mbps. This powerful router, complete with dual antennas, is outfitted with a 4-Port Fast Ethernet switch for hardwired connections.  The router also supports the latest encryption technologies allowing for a safe and secure network.  

802.11n Wireless Access Point

The 802.11n Wireless Access Point (DA2155-V1) allows users to enjoy the freedom of Wi-Fi while utilizing high-speed Internet connections (up to 150 Mbps) to stream music, video chat or watch a movie.  The system is equipped with a repeater mode, called Range Extender, to boost the wireless signal to areas previously unreachable by the existing network. The Access Point is also easily installed and configured onto the home network.

To learn more about the latest desktop networking products by Legrand, visit www.legrand.us/networking.

###

About Legrand
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of $5.8 billion in 2011.  Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819). www.legrand.us

Follow Legrand on Twitter: https://twitter.com/OnQ_HomeSystems

Media Contacts:

Meredith Miller, MarketSpace Communications

(724) 778-9933   mmiller@marketspaceagency.com