COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Reduce Clutter and Maximize Performance with the New Slimline High Speed w/Ethernet HDMI Patch Cables from Legrand

Slimmer cables are ideal for patching between AV connections in tight spaces.


HDMI Slimline

HARRISBURG, Pa., June 13, 2013 – Legrand, the leader in connected home systems, today announced the release of the high performance On-Q Slimline HDMI cables, available in one, two and four meter length.

The Slimline High Speed HDMI with Ethernet cables expand Legrand’s line of On-Q HDMI cables by providing an ideal solution for the cluttered AV connection points found in the entertainment center. The cables are 75% thinner than regular HDMI cables and support numerous video signals for optimal viewing.

“As part of Legrand’s commitment to delivering easy to install and robust infrastructure solutions, we are pleased to offer these high quality accessories for AV connectivity,” said Fritz Werder, VP and General Manager, Legrand Home Systems Division.

Available in one, two and four meter (3.3, 6.6 and 13.1 feet) length the AC3M01-WH-V1, AC3M02-WH-V1 and AC3M04-WH-V1 cables offer a reduced profile to streamline patching between various AV components, decreasing rack mount clutter. In addition, the four-meter cable is equipped with RedMere technology to allow High Speed HDMI with Ethernet performance over the longer distance.

Don’t let their size be deceiving, these powerful cables deliver uncompressed HD video and digital audio while also supporting 1080P, Ultra HD (4K) and 3D video. Additionally, the Slimline cables have Audio Return Channel and HDMI Ethernet Channel (HEC) capabilities.

To learn more about the Slimline HDMI cables by Legrand, visit www.legrand.us/audio-video/home-theater.aspx.

###

About Legrand
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of $5.8 billion in 2011.  Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819). www.legrand.us

Follow Legrand on Twitter: https://twitter.com/OnQ_HomeSystems

Media Contacts:

Meredith Miller, MarketSpace Communications

(724) 778-9933   mmiller@marketspaceagency.com

Terry Kraft, Legrand Home Systems Division

(717) 546-5406   terry.kraft@legrand.us