COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand Answers Call for Greater Network Capacity with 24-Port Gigabit Ethernet Switch


MIDDLETOWN, Pa., October 28, 2014 – Responding to the need for infrastructure to effectively support the increase in networked devices being used in homes and small businesses, Legrand, the global specialist in electrical and digital building infrastructures, has introduced the DA2524 Gigabit Ethernet Switch. Providing high speed Ethernet to as many as 24 devices simultaneously, the Gigabit Switch offers installers and distributors a valuable networking solution for new installations and retrofits.  The DA2524 is available now.

“The number of connected devices used in homes today is continuing to expand, and we are seeing more rack-based networks supporting them,” said Fritz Werder, VP & General Manager, Nuvo/On-Q.  “The DA2524 is a versatile, rack-mountable solution that installers can rely on to help them meet their customers demands.”

According to Werder, the throughput capacity and simplicity of installing the DA2425 makes it a perfect solution for future-proofing large networks being installed in homes or light commercial buildings.  Each DA2425 provides a total switching capacity of 48 Gbps, with 2 Gbps throughput per port in full duplex mode.  It automatically determines the fastest possible transmission speed for each connection, features LED indicators that confirm a connection for each network stream, and offers increased energy efficiency with power saving modes on each connection.

For installation flexibility, the DA2524 ships with mounting ears for a standard 19" rack, as well as with rubber feet for placement on a shelf or desktop.  It is UL listed and compliant to FCC, CE and RoHS standards.

 

 

 

About Legrand

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of close to $5.8 billion in 2012. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819).www.legrand.us

 

#  #  #

Link to Images

            DA2524 24 Port Gigabit Ethernet Switch Front Panel

DA2524 24 Port Gigabit Ethernet Switch Back Panel

DA2524 24 Port Gigabit Ethernet Switch Front Angle

 

Media Contact:

Roher Public Relations

Torin Roher

971-266-8870

troher@roherpr.com