COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand Adds New Active High-Speed Hdmi Cables to Support 4k/Ultra Hd Uncompressed Signals


DALLAS, October 15, 2015 – Legrand, the global specialist in electrical and digital building infrastructures, has added two new Active High-Speed HDMI With Ethernet Cables to its On-Q product portfolio that will support data speeds up to 18.6 Gigabits per second (Gbps), supporting the full requirements of 4K/UltraHD video and uncompressed HD audio.  The company also announced the additional of bulk pack cables ties, to better support its distributors.

The two new active cables are equipped with Redmere chipsets to ensure signal integrity and support both the Audio Return Channel and Ethernet connectivity.  The new cables become part of Legrand’s broader line of high speed, tri-rated HDMI cables, meeting CMG, FT4, and CL3 rating specifications for in-wall use in both residential and commercial applications throughout the USA and Canada. All compliance designations are clearly marked on the outer jackets for easy verification. The company also offers a line of Slimline high-speed active cables that are designed to be more flexible in tight spaces and thinner to minimize the outside the wall appearance.  

“Legrand is committed to providing our integrators and installers with everything they need to get their jobs done right. We will continue to extend our cables & accessories offering to give them products that ensure compliance with the latest standards and are easy for them to source,” said Fritz Werder, VP and general manager of Legrand’s On-Q and Nuvo lines. 

Legrand’s new cable ties come in three lengths and two colors: 4.75-inch, 7.5-inch and 11-inch ties in both black and natural. The high-strength, low-profile cable ties help keep wires and cables neat and orderly for superior installation. The secure notched locking prevents cable tie slippage and the small form factor head reduces cable snags and eases pulling. Each tie has a 50-lb tensile strength and is available in the both natural and black.

For more information about the new active HDMI cables or new cable ties, contact Legrand at 800-223-4162 or visit www.legrand.us.

 

About Legrand
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of close to $5.8 billion in 2012. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819).www.legrand.us

 

###

 

Links to Images:
    4K/UHD HDMI Cables With Rating Labels
    4K/UHD HDMI Cables with Connector Ends 

 

Media Contact:

Roher Public Relations
Torin Roher / Bennie Sham
971-266-8870 / 212-808-4904
legrand@roherpr.com