COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

LEGRAND SHIPS OUTDOOR IP DOME CAMERA, NETWORK VIDEO RECORDER AND APP; OFFERS AUTOMATIC EMAIL ALERTS

Components Work Day and Night to Send Pictures and Live Video Feeds


DALLAS, September 14, 2016 – Legrand, the global specialist in electrical and digital building infrastructures, announced the availability of its On-Q outdoor IP Dome Camera, network video recorder (NVR) and app that provide 24-7 viewing for the home.

Designed for operation in any space, including areas of total darkness, the On-Q IP Dome Camera is triggered by motion sensors to take pictures automatically and send them as e-mail alerts to the homeowner. Once alerted, or at any other time, users can log into the camera via the On-Q IP Camera App to observe what’s occurring on their property via live video feeds. In addition to standalone use with the app, the camera can be integrated into the On-Q Intuity home automation system for an even more powerful home surveillance solution.

“The On-Q IP Dome Camera, NVR and app give homeowners piece of mind regarding the safety of their home and family with automatic alerts and immediate viewing of their property day or night,” said Fritz Werder, Legrand VP/general manager, On-Q and Nuvo product lines. “With it, users can quickly determine if there is a threat and if any action is required.”

Because of the importance of having a visual record of events for security purposes, Legrand will also be shipping the On-Q NVR (network video recorder), which can power and record from up to four IP cameras, in October. It also sends and receives triggers from a home’s security panel to manage monitoring and sound alerts as appropriate.

The On-Q NVR is designed specifically for residential use, and it is easily configurable through a web-based interface and an HDMI connection to a four-camera HDTV display. It also natively mounts in structured wiring enclosures.

Users can also set recording schedules and view activity remotely via the free enhanced Legrand IP camera app that will soon be available from Google Play and the App Store.

For more information on Legrand On-Q IP Dome Camera, NVR and app, please click here.

About Legrand

Legrand is the global specialist in electrical and digital building infrastructures.  Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide.  Innovation for a steady flow of new products with high added value is a prime vector for growth, including in particular connectable products enhancing value in use. Legrand reported sales of $5.3 billion in 2015.  Legrand has a strong presence in North America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, QMotion, Quiktron, Raritan, Vantage, Watt Stopper, and Wiremold.  Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819). www.legrand.com. 

#  #  #


Media Contacts:

Feintuch Communications
Doug Wright / Richard Roher                                                 
212-808-4903 / 212-808-4902
legrand@feintuchpr.com