COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

ON-Q RADIANT® SELECTIVE CALL INTERCOM UNIT, FOUR-ROOM INTERCOM KIT BRING NEW LEVEL OF COMMUNICATIONS TO THE HOME


MIDDLETOWN, Pa., September 6, 2016 – Legrand, the global specialist in electrical and digital building infrastructures, introduced the radiant® Selective Call Intercom system that brings a new level of convenience and style to room-to-room communication for up to 32 locations.  The system is based on the Model IC7001 room unit, which is available individually and in a four-room kit (Model IC7400) that offers an ideal starting point for a best-in-class intercom system.

“The radiant Selective Call intercom adds to the general convenience of room-to-room communication with intuitive features that enable easier control with an LCD display & hands-free call reply,” said Fritz Werder, VP/GM for the company’s Nuvo and On-Q product lines. “It is not only a strong extension of our line of intercom and video door entry components, it is fully compatible with Intuity, our modular, enclosure-based home automation system.”

The IC7001 radiant Selective Call Intercom Room Unit delivers room-to-room communication from an in-wall control point. It offers intuitive navigation and use via its high-resolution LCD screen, along with customizable room naming, room grouping (for calling multiple rooms at once) and monitoring features.  In addition, advanced features include hands-free call reply, and do not disturb and mute options that enable users to bypass distractions when they do not wish to be interrupted.

The On-Q radiant Selective Call Intercom was designed to integrate seamlessly into Legrand's Intuity Home Automation system, which offers a complete home control solution for comfort, security, and entertainment.

This IC7400 radiant® Selective Call Four-Room Intercom Kit is the perfect starting point for installers to offer customers a best-in-class intercom system. The IC7400 is easy to set up, with no programming necessary, and provides all the components needed to outfit a four-room intercom system, including four Selective Call Room Units, four 2-gang radiant screwless wall plates, one 8-location distribution module and one 30 watt power supply.

With the addition of the optional Video Door Unit, users can also answer the door via the system.

As part of the radiant® collection of switches, outlets, dimmers and home automation controls by Legrand, this product delivers a clean and consistent look in a variety of colors and metallic finishes.

For additional information about the On-Q radiant Selective Call intercom unit (IC7001) and four-room intercom kit (IC7400), please click here.

About Legrand

Legrand is the global specialist in electrical and digital building infrastructures.  Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide.  Innovation for a steady flow of new products with high added value is a prime vector for growth, including in particular connectable products enhancing value in use. Legrand reported sales of $5.3 billion in 2015.  Legrand has a strong presence in North America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, QMotion, Quiktron, Raritan, Vantage, Watt Stopper, and Wiremold.  Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819). www.legrand.com. 

#  #  #

 

Media Contacts:

Feintuch Communications
Richard Roher / Doug Wright                                                 
212-808-4902 / 212-808-4903
legrand@feintuchpr.com