COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Ortronics/Legrand Introduces Mighty Mo® 10


New London, CT, January 11, 2008 - Ortronics/Legrand, a global leader in high performance copper, fiber and wireless structured cabling solutions, will introduce the Mighty Mo® 10 advanced cable management system at the BICSI Winter Conference, January 13 - 16 at the Gaylord Palms Convention Center in Orlando, Florida.

Specifically designed for higher density applications, such as data centers and storage area networks, the new cable management system features the Mighty Mo 10 cable management rack, which is designed to maximize the airflow of network equipment. Honeycomb side rails and baffles work together to manage intake and exhaust air, creating cold aisle/hot aisle air distribution from side vented equipment. Available in 7' or 8' heights, the Mighty Mo 10 can be assembled as a 19" or 23" rack, has a 16.25" channel depth and can fit on a 2' x 2' floor tile. Its patented construction has built-in strain relief, bend radius control and efficient patch cable routing with floor and ceiling access to distribution cables. Optional vented double hinged front and rear doors are also available for additional security.

The Mighty Mo 10 cable management system also includes a server rack that is compatible with all Mighty Mo 10 and Mighty Mo 6 racks and cable management. It is a 7' high, four-post aluminum frame with mounting rails that adjust from 12.5" to 30", even after the rack is installed.

The system also features the signature Mighty Mo vertical cable management cage with door. Its design promotes efficient routing of patch cables between racks, and the hinged door allows easy access for moves, adds and changes and creates a finished look for data center installations.

Visit Booth #1805 at the BICSI Winter Conference to see the new Mighty Mo 10 advanced cable management system.