NEWS: Legrand to acquire Universal Electric Corporation
Global leader in the development of flexible, customizable power distribution systems and manufacturer of STARLINE and U-S Safety Trolley suites of products.
Menu
Search
Menu
RSS Feed

Legrand | Ortronics Introduces New Range of Mighty Mo® Wall Mount Cabinets with Advanced Cable Management


New London, CT, January 13, 2010 – Legrand | Ortronics, a global leader in high performance network infrastructure solutions, introduces a new range of Mighty Mo® wall mount cabinets designed with advanced cable management to help secure, support, and organize networking equipment where floor space is limited or in open office environments.

The new Mighty Mo wall mount cabinets provide capacity for both active and passive equipment, and ensure maximum network performance by providing complete cable management. The cabinets feature rack unit finger style vertical managers and one pair of fully adjustable 12-24 EIA mounting rails to provide the same level of support as a full size cabinet.

Designed for maximum flexibility and ease of use, the cabinets are available with an optional rear horizontal mount bracket kit, which is designed to provide additional fixed rack units on the rear wall for vertically mounting fiber cassettes, active equipment, or power distribution units. The center section of the cabinet swings out to provide easy access to terminations without disrupting the rear wall equipment. A front lockable wing turn latch secures the front door without having to lock the cabinet, which allows for easy access into the front of the cabinet when used in a secure environment.

Mighty Mo wall mount cabinets are supplied with a variety of cable access options. Both the top and the bottom of the rear section have a 3” access hole with cap that is removable only with access to the inside of the cabinet. The top of the rear section comes standard with two brush cable entry plates to protect the cabinet from dust and dirt, and the bottom of the rear section comes standard with two knock-out plates.

The cabinets are built with a rugged 14 GA steel construction to minimize sagging under heavy loads. They are available in depths of 20" and 26" and heights of 23.50", 35.75" and 48", which provide 12, 19 and 26 rack units of equipment room. An optional 50 cfm fan provides 50% less noise than most other leading cabinets.

The new Mighty Mo wall mount cabinets are part of the Ortronics family of Layer Zero™ physical support solutions. Ortronics Layer Zero solutions maximize network efficiency by reducing power consumption and cooling costs, reducing the risk of equipment failure, and enhancing overall system performance.

###

For more information contact:
Legrand | Ortronics, 125 Eugene O'Neill Drive, New London, CT 06320
Sales: 860-445-3900 or 800-934-5432, Fax: 888-282-0043 or 860-405-2992
E-mail: connect.ortronics@legrand.us, Internet: www.legrand.us/ortronics

Editorial Contact and Photos:
Laura Fradette, Marketing Communications Manager
Legrand | Ortronics, 125 Eugene O'Neill Drive, New London, CT 06320
Direct Tel: 860-405-2861, Fax: 860-405-2972
E-mail: laura.fradette@legrand.us

Background for Editors:
Legrand | Ortronics (www.legrand.us/ortronics), headquartered in New London, Connecticut, USA is a global leader in high performance network infrastructure solutions, offering a complete range of Category 5e, 6 and 10 Gig copper, fiber optic, and residential/MDU connectivity solutions, as well as Layer Zero™ physical support solutions including Cablofil® wire mesh cable tray and Wiremold® pathways.

Legrand | Ortronics is part of Legrand, the global leader in products and systems for electrical installations and information networks where people live and work. Employing over 33,000 people worldwide, Legrand reported net sales exceeding $5.8 billion in 2008. The company holds over 5,000 active patents, with nearly 170,000 catalog items divided into 95 product families. Legrand has a strong presence in the North American market, with a portfolio of products that includes Cablofil, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is actively expanding its market divisions that include Electrical Wiring Systems, Home Systems, Lighting Controls and Commercial Datacom. Committed to providing a steady flow of innovative new products with high added value, Legrand invests 4-5% of sales in R&D. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for suppliers worldwide. Legrand is listed on Euronext Paris and is a component stock of indexes including the SBF120, FTSE4Good and MSCI World (ISIN code FR0010307819). www.legrand.us