COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand | Ortronics Introduces Mighty Mo Air Control Solutions

Passive air control: the most energy efficient method of controlling airflow and temperature in the data center


Passive air control: the most energy efficient method of controlling airflow and temperature in the data center

New London, CT, March 8, 2011 – Legrand | Ortronics, a global leader in high performance network infrastructure solutions, introduces Mighty Mo® Air Control solutions to enhance the separation between the hot and cold aisles - a crucial aspect of best practice airflow design within a data center. The Mighty Mo Air Control passive system improves air flow and optimizes thermal management without adding active cooling equipment, avoiding additional energy costs for cooling.

The cold air containment solutions include, among other products; hanging curtains, retractable aisle covers, compressible plugs and end aisle doors; all designed to eliminate the mixing of hot and cold airflow.

The Air Curtain System has fire resistant vinyl panels that hang from aluminum tracks mounted to the drop ceiling grid above racks and cabinets. The aluminum tracks connect to the ceiling grid by fusible links that release and drop to the floor when temperatures go above 135°F, ensuring that the fire sprinkler pattern is not interrupted. The curtains are available in widths from 12” to 72” and lengths from 29” to 182”.

The Air Cap is a flat, retractable roof system that attaches to the top of racks or cabinets. This retractable cover is held in place with thermal links that release the cover if temperatures go above 135°F. The fire resistant cover is spring loaded and retracts back into the metal cassette during a fire event, also ensuring that the sprinkler pattern is not interrupted and preventing the cover from being exposed to the fire. The cap is available in two sizes: 60” x 30’ and 84” x 30’.

Air Plugs are used to fill in cable openings in the raised floor or any gaps where airflow needs to be blocked. Air Plugs are fireproof, compressible and safe to use around all types of cable, including fiber optic cable. The Air Plugs are available in several sizes to cover most any opening.

Air Doors install at the end of the aisle and are available as a sliding or hinged opening. The door frame is constructed of extruded aluminum and supports clear acrylic sliding doors, bridging an aisle up to 84” wide. The doors ship fully assembled.

Mighty Mo Air Control is part of Layer Zero™. Layer Zero is the proposed infrastructure layer for the ISO/OSI model introduced by Legrand | Ortronics. Layer Zero - the Infrastructure Layer™ - addresses the critical role that the physical infrastructure plays in network performance.
Layer Zero solutions encompass the entire physical infrastructure that supports your network, including aisle containment, racks, cabinets, advanced cable management, pathway solutions, underfloor and overhead systems. By recognizing the importance of the underlying infrastructure layer and emphasizing best practices in pathway and physical support design, a new level of stability can be created for the network.

For more information on the Mighty Mo Air Control product family, visit www.legrand.us/ortronics/air-control

###


Editorial Contact and Photos:
Debbie Harris, Marketing Communications Manager
Legrand | Ortronics, 125 Eugene O'Neill Drive, New London, CT 06320
Direct Tel: 860-405-2837, Fax: 860-405-2972
E-mail: debbie.harris@legrand.us

Background for Editors:
Legrand | Ortronics (www.legrand.us/ortronics), headquartered in New London, Connecticut, USA, is a global leader in high performance network infrastructure solutions, offering a complete range of Category 5e, 6 and 10 Gig copper, fiber optic, and residential/MDU connectivity solutions, as well as Layer Zero™ physical support solutions including Cablofil® wire mesh cable tray and Wiremold® pathways.

About Legrand:
Legrand is the global specialist in products and systems for electrical installations and information networks where people live and work. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for suppliers worldwide. Legrand has a strong presence in the North American market, with a portfolio of products that includes Cablofil, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is actively expanding its market divisions that include Electrical Wiring Systems, Home Systems, Lighting Controls and Commercial Datacom. Innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $5.0 billion in 2009. The company is listed on Euronext and is a component stock of indexes including the SBF120. FTSE4Good, MSCI World and ASPI (ISIN code FR0010307819). www.legrand.us