COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand Renames its Product Family of Fiber Solutions Infiniumâ„¢

And Launches the Most Reliable and Stable Field Installable Connector


NEW LONDON, Conn., June 30, 2014 – As your networks rapidly migrate to higher bandwidth over increased distances, you need quick and easy-to-deploy solutions and future-proof designs from a brand you can trust.   At Legrand, we strive to deliver solutions designed to be better, creating increased flexibility, greater efficiency and a superior network design. 

With this vision, Legrand has renamed the complete product family of fiber solutions under the name InfiniumTM, offering a complete line of products and systems ranging from high density fiber modules, field installable connectors, cassettes and adapters to patch cords and harnesses, as well as fiber enclosures and trunk cables.  This complete set of solutions provides the highest level of performance that the Ortronics product line is known for and unsurpassed integration with the rest of the physical infrastructure offering, such as racks, cabinets and cable management.

In a constant pursuit for innovation, Legrand also announces their newest product, The Infinium field installable connector.  The connector uses index matching gel and a mechanical splice in the connector housing to make the highly reliable and stable connector.  The Infinium field installable connector requires no special tools for installation, and terminates in less than 2 minutes.  The connector is available in LC or SC with either laser-optimized 50 micron or single mode fiber.

The clip that holds the mechanical splice open for field fiber insertion doubles as a visual fault locator (VFL) window.  When connected to a VFL, the light shines brightly through the window on the clip.  Once the field fiber is installed, the VFL light travels up the field fiber and the light in the window disappears, indicating a good connection. If a connector tests too high, it is easy to re-insert the clip and re-make the connection.  No more cutting off scrap connectors and installing another.

Features of the Infinium field-installable connector:

  • No epoxy, polishing or fusion splicing required
  • Reusable termination capability (up to 3 times)
  • VFL window for proper installation
  • No special tools or skills required
  • Fast installation – Installs in less than 2 minutes
  • Factory prepared and verified end face
  • 50 micron LOMF and single-mode versions available
  • Unlimited shelf life
  • Backed by the nCompass™ warranty
  • 5-year product warranty

 

“Utilizing advanced laser interferometry equipment to monitor the manufacturing process, Infinium™ pre-polished field termination connectors exhibit highly controlled end-face geometry resulting in reliable, low insertion loss and minimal return loss connections” says Michael Wood, Product Manager for fiber solutions.  “This approach eliminates imprecise epoxy application, time consuming curing and highly variable hand polishing from field installation practices. The net effect is reduced installation expense, higher yield field terminations and better performance.” Adds Mr. Wood.

# # #

About Legrand
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of close to $5.8 billion in 2012. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, NuVo, On-Q, Ortronics, Pass & Seymour, Vantage, WattStopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819). www.legrand.us