COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand/Pass & Seymour Introduces Isolated Ground GFCI


SYRACUSE, N.Y., October 13, 2011 – Legrand/Pass & Seymour (P&S), a leading provider of electrical wiring devices and home systems, announces the availability of the first Isolated Ground GFCI Receptacle. Designed to meet the needs of expanded National Electrical Code® (NEC) requirements for GFCI protection, the Isolated Ground GFCI minimizes electrical interference from a building’s ground system.


Computers and other electronic equipment are increasingly common and can be sensitive to electrical interference.  The NEC has expanded requirements for GFCI protection onto circuits that serve this equipment, most of which require isolated ground protection to protect from electrical interference.  Two examples are cash registers in fast food restaurants and computerized equipment in labs. Installations such as these drive the need for Isolated Ground GFCI Receptacles.


“The P&S Isolated Ground GFCI is the best way to meet this increasing demand for isolated ground and GFCI protection on the same circuit” said Bill Timmons, marketing manager of residential products for Legrand/Pass & Seymour.


The Isolated Ground offering includes 15A and 20A Tamper-Resistant Duplex Receptacles. Hospital Grade models are available.  All devices have a high-impact-resistant, thermoplastic construction for superior strength and durability. An LED Trip Indicator light makes it easy to identify a tripped condition, while P&S patented SafeLock™ Protection shuts off power to the receptacle if there’s a ground fault, if there’s a miswire, or if GFCI protection is compromised.


P&S invented the first GFCI Receptacle in 1971.


To learn more about the Isolated Ground GFCIs, contact your Legrand/Pass & Seymour representative.
Legrand/Pass & Seymour is a leading provider of electrical wiring devices and accessories in North America. For more information, call 1-800-776-4035 or visit www.legrand.us.

###

About Legrand
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Named to Forbes’ 2011 list of the 100 Most Innovative Companies, Legrand believes innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $5.7 billion in 2010.  Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the SBF120, FTSE4Good, MSCI World, ASPI. In 2010, Legrand was added to the European DJSI as well (ISIN code FR0010307819).  www.legrand.us