COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

LegrandĀ® Introduces New Night Lights

Safety, durability and energy efficiency are key aspects of the new night lights


SYRACUSE, N.Y. (May. 16, 2014). – Legrand, a leading provider of electrical wiring devices and home systems, today announced the extension of its Pass & Seymour® Nightlight line with the introduction of four new products.
They include three 15Amp versions - P&S Duplex Decorator Tamper-Resistant Receptacle with Nightlight, P&S Single Pole/3-Way Switch with Nightlight and the P&S Tamper-Resistant Receptacle with Nightlight. A standard P&S Full Nightlight is also available.
All have a sensor that automatically controls the Nightlight based on the amount of ambient light available and an innovative Soft Glow energy efficient LED light that is cool to the touch with a significant lifespan of more than 20 years. The 120/125V lights are also cULus compliant.
The Duplex Decorator Tamper-Resistant Receptacle with Nightlight, Full Nightlight and Single Pole/3-Way Switch with Nightlight versions have four adjustable light settings - Off, Ultra Low, Low, Medium and High. The Tamper-Resistant Receptacle with Nightlight features a standard factory set light level. 
The two outlets on the Duplex Decorator Tamper-Resistant Receptacle with Nightlight and the single outlet on the Tamper-Resistant Receptacle with Nightlight contain Tamper-Resistant shutters that prevent the insertion of foreign objects.  In addition, all the Night Lights have a sealed design which also helps to prevent tampering.

“Not only do the new Nightlights boost the safety of a home for seniors by decreasing the chance of tripping over objects that may be undetectable in the dark, but they also keep children safe by reducing their ability to insert foreign objects in the outlets,” said Thomas Roy Sr., product line manager, Legrand Electrical Wiring Systems Division. “They are perfect for bathrooms, hallways, stairs, kitchens and nurseries.”
The Duplex Decorator Tamper-Resistant Receptacle with Nightlight and Full Nightlight both ship with optional louvers and the Single Pole/3-Way Switch with Nightlight is available in one SKU.
The Nightlights are available in a variety of colors including black, white, light almond and ivory.
The new Pass & Seymour Night Lights are available in the United States and Canada.

# # #
Connect with Legrand on Facebook www.facebook.com/legrandna, Twitter www.twitter.com/passandseymour or www.twitter.com/legrandna, and YouTube www.youtube.com/legrandna

# # #
About Legrand 
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of close to $5.8 billion in 2012. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, NuVo, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819). www.legrand.us