COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand Introduces New Range of Recessed TV Boxes

Perfect for New and Old Work Applications


SYRACUSE, NY, January 27, 2014—Legrand, a leading provider of electrical wiring devices and home systems, today announced the availability of its new range of Pass & Seymour® Recessed TV Boxes.

The new boxes are designed to provide a snug-to-wall placement for New and Old Work applications in the hospitality, education, commercial and residential environments. They are ideal for flat-screen TVs and reducing the clutter associated with a variety of cabling. Plugs and multimedia connections are conveniently recessed behind the wall surface.

“The new range of Recessed TV Boxes have steel electrical boxes that accept conduit, and all products are designed to fit in a standard 2x4 wall cavity,” said Thomas Roy Sr., product line manager, Legrand Electrical Wiring Systems Division. “The TV2MW has a unique bracket that allows face or side mounting. This means that, if desired, two boxes could be mounted—one on each side of the same steel stud.”

Four versions of the Pass & Seymour® Recessed TV Boxes are available. These include one New Work Box and three Old Work Boxes.

The New Work Boxes are aimed at new commercial construction projects. The two-gang Boxes are constructed from factory-assembled steel and contain an integral 35 cubic inch electrical box. It comes with an adjustable trim ring that is suitable for various thicknesses of wall board. There is no field assembly required.

The Old Work Boxes are designed for remodeling jobs updating spaces to take advantage of wall-mounted TVs in an existing wall. There are single-gang and three-gang models with metallic electrical boxes. They are available in kits that include surge-protection devices, wall plates, screwless finish plates and low voltage connectors. They have a molded-in rectangular cut-out template to make installation easy and fit in a standard 2x4 wall cavity.

# # #

Connect with Legrand/Pass & Seymour on Facebook/Legrandna, Twitter/passandseymour and YouTube/Legrandna


# # #

About Legrand

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of close to $5.8 billion in 2012. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, NuVo, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819). www.legrand.us