COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed
NEWS
1 - 5 of 8 articles

LEGRAND® EXPANDS INDUSTRIAL WATERTIGHT PRODUCT LINE

SYRACUSE, NY, December 2, 2015—Legrand, a leading provider of electrical wiring devices and home systems, today announced the expansion of its Pass & Seymour® industrial watertight product line with new products designed to safety in a variety of harsh applications.

UL and NEMA announce revisions to UL 943 GFCI Standard

Auto-monitoring and end-of-life power denial requirements added to UL 943 Standard
UL (Underwriters Laboratories) with the National Electrical Manufacturers Association (NEMA) announce changes to the UL Standard 943 Standard for Safety for Ground-Fault Circuit Interrupters (GFCIs) (Tri-national harmonized UL 943/CSA C22.2 No. 144.1/ANCE NMX-J-520) that will take effect on June 29, 2015. To maintain certification, all manufacturers must meet these revisions with GFCIs produced after June 28, 2015.  The current GFCIs can no longer be produced after June 28, 2015, but can be sold by manufacturers, retailers, and distributors and can be used by installers until their inventories are depleted.

Legrand® Boosts Outlet and Energy Control for Building and Facility Managers with New Plug Load RF Solution

Simple to use, easy to integrate, delivers energy efficiency
SYRACUSE, NY, May 1, 2015—Legrand, a leading provider of electrical wiring devices and home systems, today announced the availability of its new Pass & Seymour® Plug Load RF Receptacle, which provides a simple-to-use, wireless solution for plug load control.