COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand’s New Dual-Function AFCI/GFCI Receptacle Reduces Callbacks and Inventory, Saves Money


West Hartford, CT. -- November 7, 2016 -- Legrand, a leading provider of electrical wiring devices and home systems, today announced the availability of its new Pass & Seymour® Dual-Function AFCI/GFCI Receptacle.  Aimed at the residential market, the AFCI/GFCI Receptacle is the latest innovation in electrical safety, and a Code-approved alternative to AFCI/GFCI breakers.

Designed to protect against electrical fires caused by arc faults and injury due to electrical shock, these new devices are compliant with NEC® AFCI and GFCI requirements in kitchens and laundry areas for new construction, circuit modifications/extensions and replacement receptacles.

Like GFCI receptacles, AFCI/GFCI receptacles are installed at the point of use, so homeowners easily see the indicator light, and perform TEST and RESET locally. The Pass & Seymour Dual-Function AFCI/GFCI Receptacle has separate indicator lights for AFCI and GFCI, making it easy to distinguish between a trip caused by an arc fault and a trip caused by a ground fault.

Delivering AFCI and GFCI protection in a single, code-compliant device at the point of use benefits the homeowner and the contractor, according to Bill Timmons, Director of Marketing at Legrand. “The receptacle is in the living area, not out of sight, or in the basement. This means less confusion for the homeowner and easier troubleshooting and fewer callbacks for the contractor.”

Unlike AFCI/GFCI breakers, which must match the brand of the breaker box, the Dual-Function AFCI/GFCI Receptacles are universal, fitting any wall box and reducing the amount of inventory a contractor needs to carry on their truck.

The GFCI function has a self-test feature that tests itself every three seconds—instead of the industry-standard three hours—providing an unprecedented level of protection.

The Dual-Function AFCI/GFCI Receptacle, which is part of Legrand’s radiant® collection, comes with ground terminal back-wiring and two holes per termination for added flexibility and faster installation. The auto-ground clip assures a positive ground to the metal box. Each Dual-Function AFCI/GFCI Receptacle has tamper-resistant shutters and Legrand’s patented SafeLock® protection for added safety.

 

Connect with Legrand on Facebook www.facebook.com/legrandna, Twitter www.twitter.com/passandseymour or www.twitter.com/legrandna, and YouTube www.youtube.com/legrandna

###

About Legrand

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including in particular connectable products enhancing value in use. Legrand reported sales of $5.3 billion in 2015. Legrand has a strong presence in North America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, Pinnacle Architectural Lighting, QMotion, Quiktron, Raritan, Vantage, Watt Stopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819). www.legrand.com

 

Media contact:

Chuck Beeler, Eric Mower + Associates
(315) 413-4346
cbeeler@mower.com