COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand Brands WattStopper and Vantage Controls Collaborate to Launch Best-in-Class Architectural Dimming Panel Platform


Santa Clara, CA, and Orem, UT, January 6, 2016 – Legrand, North America today introduced its Lighting Control and Automation Panel (LCAP) series, an architectural dimming and integration platform designed to provide enhanced end-user experiences, comply with the latest energy codes and standards, and simplify design for future space requirements. This powerful system was developed by Legrand brands WattStopper and Vantage Controls, leaders in application expertise and scalable, effortless lighting and control solutions.

The product platform helps designers easily meet precise dimming and energy conservation objectives, and is ideal for a wide range of commercial applications including schools, office buildings, hotels, museums, and restaurants. Products in the LCAP series include lighting control panels and a range of unique interfaces. The platform can also integrate with the award-winning Digital Lighting Management System (DLM) system to deliver optimal energy performance and with A/V, shades, climate, and other systems for greater user convenience.

Easy to specify, install, commission and use, the platform adapts to changing project requirements and new complexities like LEDs. Dimming LEDs require careful coordination of lamps, drivers and controls to ensure proper performance. The LCAP panels provide modular pre-configured architectural dimming and integration options. Also, exclusive patent pending technology allows the dimming curve for each dimming channel to be independently customized for starting and stopping points as well as linearity. This means smooth dimming and consistent lighting when using mixed lighting types or brands.

The LCAP series features:

  • LCAP lighting control panels: Offers high density and fully configurable dimming for all lighting technologies. Four versions are available to meet any project from small to large spaces where sophisticated sequences of operation are required.

  • Equinox user interfaces: Empowers facility managers and end-users to create a specific mood, light the perfect scene, or emphasize specific focal points. This family of simple and intuitive interfaces allow access and control from room to multiple locations via keypads, touchscreens, or mobile apps.

  • Digital Lighting Management (DLM): Delivers a full building lighting control and energy

saving solution when integrated with the architectural dimming platform. DLM allows designers to easily layer multiple control strategies and integrate with other building systems for optimal energy performance.

"The LCAP series demonstrates our approach to deliver the ultimate in simplicity, scalability, and flexibility to controls and automation solutions,” said Andrew Wale, vice president of product marketing, Building Control Systems at Legrand. “By combining the expertise and technologies from WattStopper and Vantage Controls, we’ve created a best-in-class architectural dimming system that is designed to meet a wide range of commercial applications and fulfill project objectives whether for retrofit or new construction.”

About the Lighting Control and Automation Panel (LCAP) Series

New series of dimming panels support room to area lighting control applications. The panels offer fully configurable dimming for all lighting technologies; integration with HVAC, shades, sensor/area control and provide incomparable end-user control with unique user interface options.

About Legrand

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $6.0 billion in 2014. Legrand has a strong presence in North America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Middle Atlantic, NuVo, On-Q, Ortronics, Pass & Seymour, Quiktron, Vantage, Watt Stopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819). legrand.us

###

Editorial Contacts and Photos

Reid Cram

Vantage Controls | 1061 South 800 East Orem, UT 84097

E-mail: reid.cram@vantagecontrols.com

Mary Placido

WattStopper | 2800 De La Cruz Blvd. Santa Clara, CA 95050

E-mail:pr@wattstopper.com