text.skipToContent text.skipToNavigation

Legrand® Introduces Wattstopper® Blanco LED Light Engines for Tunable White Lighting Solutions


SAN JOSE, Calif., August 7, 2018Legrand, North & Central America today announced two new tunable white LED light engines, Blanco 2 and Blanco 3, that deliver fixture manufacturers a completely integrated solution that enables the highest quality tunable light available. Both serve as natural expansions to Legrand’s Human Centric Lighting line of products.

The Wattstopper line takes the complexity out of tunable lighting projects by providing a turnkey solution that integrates seamlessly with the Wattstopper Digital Lighting Management (DLM) platform to ensure simple, intuitive, and cost effective control.

Blanco 2 is a two-channel LED light engine solution providing high-quality light with a tunable range of 3000K-5000K. This makes it ideal for education and general lighting applications. Blanco 3 is the three-channel LED light engine solution that adjusts correlated color temperatures precisely along the blackbody locus across a wide range of color temperature to replicate natural daylight. With a tunable range of 2700K-6500K, Blanco 3 is ideal for healthcare and office applications.

Both light engines provide high quality white light with a color rendering index (CRI) and TM-30 data of at least 90 and provide flicker-free dimming from 100% to 0. 1%. Blanco light engines connect to dedicated LED arrays, which are available in Zhaga-compliant linear or custom form factors, ensuring an easier integration.

“The demand for tunable white light continues to strengthen and we’re taking human-centric lighting to the next level with these products,” says Jared Morello, Wattstopper Product Marketing Manager at Legrand. “The Blanco product family removes costly startup and commissioning that’s required by traditional tunable products. With these solutions, customers will be able to fully benefit from human centric lighting solutions without significant project price increases.”

The combination of Wattstopper lighting controls expertise and the sophisticated tunable LED light engine technology from Lumenetix delivers advanced lighting systems that are easy to design, install, and control.

 

###

About Wattstopper
Wattstopper, a product line of Legrand, offers the most comprehensive line of simple, scalable and flexible energy efficient lighting controls and solutions for commercial and residential applications. The Wattstopper range of products, programs, and services have been helping customers save energy, meet green initiatives and comply with energy codes for more than 30 years. www.legrand.us/wattstopper.

About Legrand and Legrand, North and Central America
Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $6.2 billion (USD) in 2017. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines that includes AFCO Systems, C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic Products, Milestone AV, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, Projecta, QMotion, Quiktron, Raritan, Sanus, Server Technology, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us.

Media Contact:
Mary Placido, Legrand Building Control Systems
415-218-3627 mary.placido@legrand.us