text.skipToContent text.skipToNavigation

Legrand® Launches Wattstopper® Fixture Integrated Outdoor/High Bay Sensors with Bluetooth® Commissioning


SAN JOSE, Calif., August 9, 2018 – Legrand, North & Central America today released the Wattstopper FSP-300 Series Passive Infrared Outdoor Sensor, which adds Bluetooth low energy technology communication to the industry-leading FSP family of occupancy sensors. The FSP-300 Series sensor is designed to add enhanced security while improving commissioning of lighting projects with wireless access, eliminating the need to use ladders or tools. Additionally, Bluetooth low energy technology is less susceptible to environmental interferences, providing greater installation flexibility and use in the field when compared to IR remote technologies.

Ideal for warehouse, parking, and outdoor lighting applications, this sensor provides intensity control of 0-10V LED drivers or ballasts and on/off control ofnon-dimming ballasts based on motion or daylight contribution. Additionally, photosensor and daylight capabilities add a dusk-to-dawn control option for unmatched sequence of operation flexibility. The FSP-300 Series sensors are available in three models providing different options for mounting inside a fixture, outside a fixture via 1/2” knockout, or to a pole.

The sensor can be easily set up, configured, and customized with the Legrand Sensor Configuration app, which is available on iOS and Android platforms. Sensor profiles can be created, stored, and recalled eliminating the need to input parameters each time. This, along with a host of features like “Jobsite Manager” and “Device Discovery” make configuring every job faster and easier than ever before. The app eliminates the need to purchase other remote hardware and allows contractors to get on and off the job quickly.

The FSP-300 Series sensor comes with all the features and benefits of the FSP line and now includes:

  • Security features that protect device, data, and users from unauthorized access and malicious attacks.
  • Field upgradable firmware for timely updates and features to help with future sensor improvements.
  • Code compliance with latest ASHRAE 90.1, IECC, and California Title 24 outdoor lighting control requirements.
  • IP66 rated with a choice of lenses to ensure complete coverage for mounting heights up to 40 feet.
  • 100-foot commissioning range

 “The FSP-300 Series is helping simplify an often complex commissioning process,” said Daniel Stankovich, Wattstopper Product Manager at Legrand. “For fixture manufacturers, Bluetooth low energy technology offers additional specifiable features to increase the value of their lighting fixtures. Electrical contractors will also love this sensor as they are easy to install and configure and provide greater flexibility with the ability to update sensor firmware in the field.”

For more information contact your local Wattstopper Account Manager and visit our website at legrand.us.
  

###


About Wattstopper

Wattstopper, a product line of Legrand, offers the most comprehensive line of simple, scalable, and flexible energy-efficient lighting controls and solutions for commercial and residential applications. The Wattstopper range of products, programs, and services has been helping customers save energy, meet green initiatives, and comply with energy codes for more than 30 years.legrand.us/wattstopper

About Legrand and Legrand, North and Central America

Legrand is a global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial, and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value is a prime vector for growth, including, in particular, connected devices stemming from Legrand’s global Eliot (Electricity and IoT) program. Legrand reported sales of $6.2 billion (USD) in 2017. Legrand has a strong presence in North and Central America, with a portfolio of well-known market brands and product lines that includes AFCO Systems, C2G, Cablofil, Chief, Da-Lite, Electrorack, Finelite, Luxul, Middle Atlantic Products, Milestone AV, Nuvo, OCL, On-Q, Ortronics, Pass & Seymour, Pinnacle, Projecta, QMotion, Quiktron, Raritan, Sanus, Server Technology, Solarfective, Vaddio, Vantage, Wattstopper, and Wiremold. Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating, and DJSI (ISIN code FR0010307819) www.legrand.us.
 
###
Media Contact:
Mary Placido,
Legrand Building Control Systems
415-218-3627 mary.placido@legrand.us