Join us at Greenbuild Nov 19-22, 2019 in Atlanta
Click here to register for your free floor pass today
Menu
Search
Menu
RSS Feed

LFI 2016: Legrand Demonstrates New Integrated Architectural Dimming and Shading Solutions


San Diego, CA, April 25, 2016, LIGHTFAIR International – Legrand, North America will exhibit its newest solutions from leading product lines Wattstopper, Vantage and QMotion at Lightfair International Booth #4726 from April 26-28, 2016. Legrand will present its architectural dimming and integration platform, which demonstrates how all three brands have combined their respective areas of expertise in architectural dimming, automated lighting, and shading solutions to create one ultimate system to meet customer objectives and deliver on the end-user experience.

 

Products in the architectural dimming platform include the Lighting Control and Automation Panel (LCAP) series and a range of unique interfaces and modules. The platform can also integrate with A/V, shades, climate, and other systems for greater user convenience, including the Wattstopper Digital Lighting Management (DLM) system for optimal energy performance and QMotion’s Qadvanced Intelligent System (QIS) and Qadvanced with ZigBee HA1.2 for interactive motorized shade controls. Products that will be shown include:

 

  • LCAP series: Panels offer high density and fully configurable dimming for all lighting technologies. Four versions are available to meet any project from small to large spaces where sophisticated sequences of operation are required. Exclusive patent pending technology allows the dimming curve for each dimming channel to be independently customized for starting and stopping points as well as linearity. This means smooth dimming and consistent lighting when using mixed lighting types or brands.

 

·InFusion Universal Dimming Module: This product provides effective dimming control of multiple lighting sources. A key product supporting the migration to LED lighting, the module provides exceptional support of the widest range of lighting source types and allows lighting professionals to seamlessly integrate lighting without compromising on performance. The 120V to 277V module can be mounted in an LCAP main or secondary power enclosure and controls up to eight universal loads with up to four line feeds with 32 AMPs per module. It offers load-by-load selectable load type (forward or reverse phase) and auto load-type detection.

 

“Lightfair is the premier event where companies show their best products and technologies for the year, and it’s no different for us,” said Tom Lowery, president, Building Controls Systems division at Legrand. “Exemplified by our architectural dimming platform, we continue to build on our comprehensive and proven integrated solutions to help meet every building project goal from basic code compliance to supporting advanced building networks and LED applications.”

 

For more information, please visit: http://www.wattstopper.com/lightfair.aspx.

 

 

About Wattstopper

Wattstopper, a product line of Legrand, offers the most comprehensive line of simple, scalable and flexible energy efficient lighting controls and solutions for commercial and residential applications. The Wattstopper range of products, programs, and services have been helping customers save energy, meet green initiatives and comply with energy codes for more than 30 years. www.legrand.us/wattstopper.

About Legrand

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide.  Innovation for a steady flow of new products with high added value is a prime vector for growth, including in particular connectable products enhancing value in use. Legrand reported sales of $5.3 billion in 2015.  Legrand has a strong presence in North America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, QMotion, Quiktron, Raritan, Vantage, Wattstopper, and Wiremold.  Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819). www.legrand.com.

###