COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

WattStopper Releases Next Generation Power Packs


WattStopper Releases Next Generation Power Packs

Code- and retrofit-ready BZ-200 and BZ-250 are the most feature rich and robust power packs in the market

SANTA CLARA, Calif., April 24, 2015 – WattStopper today introduced its BZ-200 and BZ-250 lighting and plug load power packs that come with features for increased performance, reliability and functionality. The new power packs are designed with installation-friendly form factor including a unique Load On/Off button that allows contractors to activate lighting or plug load immediately following installation.

Offering unparalleled flexibility, the BZ-250 with Flex Control includes voltage detection circuit technology and features for advanced sequences of operation. Its mechanically held latching relay with selectable power loss operation can be set to on, off or last state just prior to a power failure, so that lighting is in the preferred state when power is restored. It also enables Auto-On or Manual-On operation for code compliance. Hold-On and Hold-Off inputs integrate with BAS, lighting control panels and other building systems.

The BZ-200 series power packs are ideal for control of lighting, plug loads and motor loads in spaces that benefit from occupancy-based control including commercial offices, classrooms and conference rooms.

Additional BZ-200 and BZ-250 features include:

  • UL listings (UL 244A & UL 508) to control plug and lighting loads to meet code requirements
  • Tested to NEMA 410 for E-ballast and LED driver inrush current
  • Improved short circuit and thermal protection to prevent catastrophic failure
  • 12AWG line voltage leads match 20A rated building wiring and 20 Amp rating for lighting and plug loads at 120-277VAC
  • LED load status indicator

WattStopper’s next generation power packs will be featured in the WattStopper and Vantage booth #802 at LIGHTFAIR® International in New York, May 5-7, 2015.

 

About WattStopper:

WattStopper (www.wattstopper.com), a Legrand group brand, is a leading manufacturer of energy efficient lighting controls for commercial and residential use. We help customers find convenient ways to save energy, meet green initiatives, and comply with energy codes with our comprehensive range of products, programs, and services. Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, Corporate Oekom Rating and DJSI (ISIN code FR0010307819). www.legrand.com.

###

Editorial Contact and Photos:
Mary Placido
WattStopper | 2800 De La Cruz Blvd. Santa Clara, CA 95050
E-mail:pr@wattstopper.com