COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

High-Capacity Work Surface Portals


WEST HARTFORD, Conn. (March 31, 2010) – Legrand/Wiremold has introduced high-capacity work surface portals that provide convenient table-top access to electrical, voice, data, video, and audio services.  Evolution™ Series work surface portals are based on the design of the popular Evolution™ Series poke-thru device.  These robust units have the capacity to accommodate large devices and cabling, yet install unobtrusively into any table top. 

Evolution Series work surface portals differ from many table-top products in that the cover is fully closed, even when computers, projectors, and other equipment are plugged in and in use.  The cover assembly features two unique spring-loaded slide cable egress doors that provide access without using flip lids, doors, or pop-ups.  Power receptacles and voice, data, and A/V connections are mounted below the table surface, which protects the connections and minimizes obstructions on the table surface. 

Evolution Series work surface portals are available in 6" or 8" sizes. Other options include surface- or flush-style and cord-ended or hard-wired versions.  Solid, die-cast aluminum covers feature durable, powder-coated colors: nickel, bronze, brass, gray, and black. 

About Legrand/Wiremold
Legrand/Wiremold, headquartered in West Hartford, Conn., is the leader in wire and cable management systems, including metal and nonmetallic raceways, power-poles, poke-thru devices, floor boxes, Walker® underfloor systems, plug-in outlet centers, firestopping systems, and innovative architectural columns.  Please visit http://www.legrand.us/Wiremold.aspx or call 1-800-621-0049. 

About Legrand
Legrand is the global specialist in products and systems for electrical installations and information networks where people live and work. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for suppliers worldwide. Legrand has a strong presence in the North American market, with a portfolio of products that includes Cablofil, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is actively expanding its market divisions that include Electrical Wiring Systems, Home Systems, Lighting Controls and Commercial Datacom.  Innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $5.0 billion in 2009. The company is listed on Euronext and is a component stock of indexes including the SBF120. FTSE4Good, MSCI World and ASPI (ISIN code FR0010307819). www.legrand.us