COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Infloor Activation Covers are More Durable, Easier to Use


WEST HARTFORD, Conn. – Legrand/Wiremold has redesigned its FloorPort™ Series infloor activation covers to provide enhanced durability, improved function, and new designer colors.  FloorPort covers are fully compatible with new and legacy Resource RFB® Series floor boxes, and Walkercell® and Walkerdeck® systems.  These covers are designed for a wide range of applications, from schools and airports to offices and institutions.

Activation covers are subjected to considerable wear and tear from frequent opening and closing to connect power and data devices – not to mention foot traffic.  Re-engineered FloorPort covers have been improved in several ways.  A full-size handle makes the cover easy to open and close.  A more durable, one-piece articulated hinge allows the cover to open full 180° so it lies flat for less mechanical strain, easy access, and reduced trip hazards.  Egress doors have been made larger and have an automatic locking feature that prevents them from closing down and pinching wires and cables.

FloorPort covers are offered in flanged and flangeless styles, with and without cutouts for inserting flooring finishes.  A furniture feed option is also available.  Color options include nickel, bronze, brass, grey, black, and brushed aluminum.  These colors are consistent with covers for Evolution™ Series poke thru devices, floor boxes, and work surface portals.  Durable powder coat paint also reduces environmental impact.

FloorPort covers feature TopGuard™ protection that exceeds UL® scrub water standards and safeguards power and data compartments against water, dust and debris.  These covers are UL Listed to U.S. and Canadian safety standards for tile, terrazzo, carpet, and wood floors.

About Legrand/Wiremold
Legrand/Wiremold, headquartered in West Hartford, Conn., is the leader in wire and cable management systems, including metal and nonmetallic raceways, power-poles, poke-thru devices, floor boxes, Walker® underfloor systems, plug-in outlet centers, firestopping systems, and innovative architectural columns.  For more information visit www.wiremold.com or call 1-800-621-0049.

About Legrand
Legrand is the global specialist in products and systems for electrical installations and information networks where people live and work. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for suppliers worldwide. Legrand has a strong presence in the North American market, with a portfolio of products that includes Cablofil, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is actively expanding its market divisions that include Electrical Wiring Systems, Home Systems, Lighting Controls and Commercial DataCom.  Innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $5.0 billion in 2009. The company is listed on Euronext and is a component stock of indexes including the SBF120. FTSE4Good, MSCI World and ASPI (ISIN code FR0010307819). www.legrand.us