COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand/Wiremold Introduces Enclosures for Cisco® 1250 Aironet Units


WEST HARTFORD, Conn.– Legrand/Wiremold has introduced three new wireless access point (WAP) enclosures that are designed specifically for use with the Cisco® 1250 Aironet wireless access point.  These secure enclosures conceal the WAP and allow for optimal Wi-Fi signal coverage to adjacent spaces while supporting industry standard POE (power over Ethernet).  Two of these new enclosures are for drop ceiling applications, while the third is a wall-mounted unit.

WAPE5-1250KITD and 1250KITR Wireless Access Point Enclosures provide a 5" deep enclosure that fits into a 2' x 2' drop ceiling tile grid.  Faceplates allow for mounting the Aironet 1250 WAP using dipole antennas (1250KITD) or remote antennas (1250KITR).  These ceiling enclosures are plenum rated by UL and may be used in environmental air spaces. These enclosures for active equipment meet all requirements of the TIA/EIA-569-B “Pathways and Spaces” standards.

The NME1250AP Wireless Access Point Enclosure conceals wireless access points in a wall-mounted, ETL/cETL listed enclosure.  Its thermoplastic construction provides protection for expensive access point hardware and fragile antennae while allowing optimum placement for maximum signal performance while supporting industry standard POE.  Antennas for Cisco Aironet 1250 access points can be configured either internal or external to the enclosure. The enclosure can be mounted vertically or horizontally, and includes a concealed key lock under a subdoor to prevent unauthorized access.

Wiremold® wireless access point enclosures are supplied with mounting hardware, and have design features for ease of installation. 

About Legrand/Wiremold
Legrand/Wiremold, headquartered in West Hartford, Conn., is the leader in wire and cable management systems, including metal and nonmetallic raceways, power-poles, poke-thru devices, floor boxes, Walker® underfloor systems, plug-in outlet centers, firestopping systems, and innovative architectural columns.  Please visit www.legrand.us/Wiremold or call 1-800-621-0049.

About Legrand
Legrand is the global specialist in products and systems for electrical installations and information networks where people live and work. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for suppliers worldwide. Legrand has a strong presence in the North American market, with a portfolio of products that includes Cablofil, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is actively expanding its market divisions that include Electrical Wiring Systems, Home Systems, Lighting Controls and Commercial Datacom.  Innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $5.0 billion in 2009. The company is listed on Euronext and is a component stock of indexes including the SBF120. FTSE4Good, MSCI World and ASPI (ISIN code FR0010307819). www.legrand.us