COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Power Pole Extender Increases Space Flexibility, Improves Job-Site Efficiency


WEST HARTFORD, Conn. (June 3, 2010) – Legrand/Wiremold now makes it easier to install power poles, including making on-site modifications to accommodate a variety of height requirements.  Wiremold® Tele-Power® Pole Extenders are available in 5-foot sections that snap together to create a single standard pole – or they may be used to extend the length of an existing pole. 

Dual-compartment Tele-Power Pole Extenders work with standard Wiremold 25 Series Tele-Power Poles to provide up to five feet of additional height.  The Tele-Power Pole Extender, which can be cut to length, slips securely onto the original pole.  A patent-pending mounting system ensures that the finished pole is as strong and durable as a single unit. 

Legrand/Wiremold also offers prewired and unwired Tele-Power Pole Extenders that can be combined in the field to make a single 10-foot pole.  Factory-wired units come with two 20A, 125V duplex receptacles.  Wired and unwired units are supplied with mounting hardware, end plate, and ceiling trim. 

Tele-Power Pole Extenders offer numerous advantages over longer, single units.  They are shipped in smaller packages, so they are easier to handle and store on site. In addition, smaller units are less likely to be damaged during shipment.  For last-minute changes, Tele-Power Pole Extenders can be shipped by air or ground, and are stocked by Wiremold distributors. 

About Legrand/Wiremold
Legrand/Wiremold, headquartered in West Hartford, Conn., is the leader in wire and cable management systems, including metal and nonmetallic raceways, power-poles, poke-thru devices, floor boxes, Walker® underfloor systems, Plug-in Outlet Center® units, firestopping systems, and innovative architectural columns.  Please visit http://www.legrand.us/Wiremold.aspx  or call 1-800-621-0049.

About Legrand
Legrand is the global specialist in products and systems for electrical installations and information networks where people live and work. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for suppliers worldwide. Legrand has a strong presence in the North American market, with a portfolio of products that includes Cablofil, On-Q, Ortronics, Pass & Seymour, Vantage, WattStopper and Wiremold. The company is actively expanding its market divisions that include Electrical Wiring Systems, Home Systems, Lighting Controls and Commercial Datacom.  Innovation for a steady flow of new products with high added-value is a prime vector for growth. Legrand reported sales of $5.0 billion in 2009. The company is listed on Euronext and is a component stock of indexes including the SBF120. FTSE4Good, MSCI World and ASPI (ISIN code FR0010307819). www.legrand.us