COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

New Plugmold Multioutlet Strips Combine Tamper-Resistant Receptacles and a Thin Profile


WEST HARTFORD, Conn., January 11, 2011 – Legrand/Wiremold has introduced a new Plugmold multioutlet strip that integrates tamper-resistant receptacles into a low-profile unit that provides more access to power anywhere in the home. The Plugmold 2000TR Series Multioutlet System employs patented internal shutters to prevent insertion of unwanted objects into the receptacle. It meets the requirements of 2008 NEC section 406.11, which requires tamper-resistant receptacles in dwelling units.

As homes require more access to power, surface mounted multioutlet strips provide added convenience in kitchens, home offices, workshops, and garages. Until now, however, the tamper-resistant feature was available only in larger profile products. The thinner size of the Plugmold 2000TR Series meets all requirements without sacrificing style. Color options include ivory, gray, white, black and stainless steel and anodized aluminum finishes.

Plugmold 2000TR Series multioutlet strips are available in or steel or aluminum in standard 3' and 5' lengths with 6" outlet spacing. These surface-mounted units install in minutes, without breaking into the wall and pulling wires.


About Legrand/Wiremold
Legrand/Wiremold, headquartered in West Hartford, Conn., is the leader in wire and cable management systems, including metal and nonmetallic raceways, power-poles, poke-thru devices, floor boxes, Walker® underfloor systems, plug-in outlet centers, firestopping systems, and innovative architectural columns. Please visit http://www.legrand.us/Wiremold.aspx or call 1-800-621-0049.


About Legrand
Legrand is the global specialist in products and systems for electrical installations and information networks where people live and work. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for suppliers worldwide. Legrand has a strong presence in the North American market, with a portfolio of products that includes Cablofil, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is actively expanding its market divisions that include Electrical Wiring Systems, Home Systems, Lighting Controls and Commercial Datacom. Innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $5.0 billion in 2009. The company is listed on Euronext and is a component stock of indexes including the SBF120. FTSE4Good, MSCI World and ASPI (ISIN code FR0010307819). www.legrand.us

###