COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

New Wiremold Flat Screen Wall Box


EFSB4 with module being installed

WEST HARTFORD, Conn., September 4, 2013 –  Legrand has introduced a Wiremold® in-wall device box to provide power, communications and audio/video to wall-mounted flat screen monitors. The Evolution™ Series Flat Screen Wall Box is available in 4-gang and 2-gang options that offer complete flexibility for any combination of connectivity devices. This box supports digital displays in conference and meeting rooms and training facilities in commercial offices, as well as education, medical, and other institutions.

The Evolution Series Flat Screen Wall Box features unique removable device modules that support industry-standard device plates that can be detached and removed for easier installation by multiple trades and to facilitate moves, adds and changes as services do not need to be entirely disconnected and reconnected.  The 4-gang box holds two device modules. The 2-gang version has one module with storage space for active A/V components. All modules have a removable divider for separation of power and low-voltage service.

“Legrand developed this new box to meet the growing use of flat screens for multiple purposes, including digital signage,” said Michael Cole, Legrand Product Marketing Manager. “This box supports the full range of communications, while also keeping the screen as close as possible to the wall, which is a major customer concern.”

The Evolution Series Flat Screen Wall Box installs in steel and wood stud walls in new construction or retrofit projects.  Conduits knock-outs from ¾" to 2" and 3 ½" of space behind the device plates make installation easier and faster. Integral tunnels on both sides of the device modules enable wire and cable to pass through.  The interior of the box is painted white for improved visibility.

About Legrand 

Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of $5.8 billion in 2011. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed as LR.PA (PARIS: LR) on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819). www.legrand.us  

 

Follow Legrand on Twitter: http://twitter.com/legrandna

# # #

 

Media contact:

Bill Graulty
(860) 679-9761
billg@mintz-hoke.com