NEWS: Legrand acquires Universal Electric Corporation
Global leader in the development of flexible, customizable power distribution systems and manufacturer of STARLINE and U-S Safety Trolley suites of products.
Menu
Search
Menu
RSS Feed

Legrand Expands Line of Wiremold Plug-in Outlet Centers


Medical/Dental Grade / APPROVED for Patient Care Areas / 120V/20A / 6 O/L / 6

WEST HARTFORD, Conn., Mar. 1, 2013 – Legrand has introduced several new Wiremold® Plug-in Outlet Centers that provide surge protection for office, commercial, school and medical applications. “We continue to add features in response to today’s commercial and institutional environments, and to meet our customers’ needs,” said Jim Forte, P.E., Legrand Compliance/ Product Marketing Manager. New Plug-in Outlet Center products include:

Network Surge Protection: Perma Power® M6BZNET and M6BZNET-15 computer grade surge protectors not only protect the 120V power line but also connected computer networks. Laptops and desktops are protected by an integrated network surge protector to stop surges on the RJ-45 network lines. Two of the six outlets are spaced for plug-in transformers so an outlet is no longer blocked when a plug-in transformer is used. Cords incorporate a 45-degree offset right-angle plug that hugs the wall without blocking the second outlet of a receptacle. These units are UL and cUL Listed and meets both UL1363 and UL1449 3rd Edition Standards for Surge Protection Devices.

Medical Grade: Wiremold ULM Series Medical Grade Plug-in Outlet Centers can be used in patient care areas in compliance with Article 517 of the National Electrical Code (NEC). These units feature redundant bonding, a rugged aluminum housing and Pass & Seymour® hospital grade receptacles.

36" Devices: Legrand has also introduced several 36" 15A Plug-in Outlet Centers to fill the gap between 24" and 48" models. These units are designed for use in relay racks and cabinets, laboratories, workshops, classrooms and offices. The UL309BC and UL309BD have nine outlets, a lighted switch, and a 6 foot and 15 foot cord respectively. The 3609ULBC and 3609ULBD join the CabinetMate® Series with nine outlets and a 6 foot and 15 foot cord respectively. These units are UL and cUL Listed to UL1363 standards. Rack-mount units are UL and cUL Recognized to UL1363 standards.



About Legrand

Legrand (www.legrand.com) is the global specialist in products and systems for electrical installations and information networks where people live and work. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for suppliers worldwide. Legrand has a strong presence in the North American market, with a portfolio of products that includes Cablofil, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is actively expanding its market divisions that include Electrical Wiring Systems, Home Systems, Lighting Controls and Commercial Datacom. Innovation for a steady flow of new products with high added value is a prime vector for growth. Legrand reported sales of $5.0 billion in 2009. The company is listed on Euronext and is a component stock of indexes including the SBF120. FTSE4Good, MSCI World and ASPI (ISIN code FR0010307819). www.legrand.us

###