COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Easy-to-Install Chargers Power up Electronic Devices, Clean up Messes

Wall-mounted units provide both outlet and USB charging


USB/Multi-Outlet Charging Station, PX1002

WEST HARTFORD, Conn., September 18, 2013Mobile phones, tablets, music players and other devices are wonderful conveniences but keeping them powered up, organized, and easy to find creates a jumble of chargers, a messy tangle of cords, and an unsightly spot that tends to attract other “stuff.” Legrand has a solution that anyone can install in minutes to increase the number of devices that can be charged at the same time, direct from a power outlet or by USB. 

 

Legrand USB/Multi-Outlet Charging Stations provide three power outlets and four USB ports so up to seven devices can receive power simultaneously. They mount flush to the wall, freeing up valuable table and countertop space.  Installation couldn’t be easier: simply remove the wall plate from an existing receptacle and install the charging station into the wall plate holes using the screws provided.

 

Legrand offers two USB/Multi-Outlet Charging Stations. Both offer 2.0 Amp USB output that is compatible with tablets, smart phones and other devices. This output will charge two to three smart phones or one to two tablets, depending on device type and battery level. These charging stations feature built-in surge protection that’s backed by a $100,000 protected equipment warranty.

 

The PX1002 USB/Multi-Outlet Charging Station creates a sleek wall-mount charging center for all mobile devices. Its padded, non-skid, slide-out side pockets provide a convenient place to store devices while they charge. It even has optional hang hooks for keys or additional cable management. The suggested retail price is $35.99.

The PX1003 USB/Multi-Outlet Charging Station features a built-in cable management reel that keeps cords organized and off the floor. The suggested retail price is $24.99.

Legrand USB/Multi-Outlet Charging Stations are available at The Home Depot and other retailers. Please visit the Legrand DIY Project Corner for more information on installing charging stations and other do-it-yourself projects.

# # #

 

About Legrand
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of close to $5.8 billion in 2012. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, NuVo, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819). www.legrand.us

 

Media contact:
Bill Graulty
(860) 679-9761
billg@mintz-hoke.com