COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed
NEWS
1 - 5 of 6 articles

New Plugmold Multioutlet Systems Offer Enhanced USB Charging

WEST HARTFORD, Conn., November 19, 2014 – Legrand has expanded its line of Plugmold® Multioutlet Systems to offer more USB charging capability. New units include all-USB options, a unit with alternating USB ports and power receptacles, and one with a single dual USB module and receptacles. These Plugmold Multioutlet Systems meet the growing demand for device charging in airport departure areas, waiting rooms, homes, and even bars – anywhere people need to charge mobile devices. All feature dual-port charging modules that share 2.4 amps of charging capacity and can charge multiple phones, tablets, or other mobile devices at the same time.

Legrand Floor Boxes are Fire Rated for up to Three Hours

WEST HARTFORD, Conn., (July 23, 2014) – Legrand now offers 19 Wiremold® flush style floor boxes that have been evaluated, tested, and approved to meet UL Fire Classification requirements for at minimum a two-hour floor rating and, in many cases, a three-hour rating. Available in both single and multiple-gang versions in steel and nonmetallic fabrications, they provide power, communication, and audio/video services into open spaces. These boxes also accept existing cover plates and service fittings to present a more consistent and aesthetic finish throughout the building.

Legrand Introduces a Broad Range of Meeting Room Solutions

Designed to help A/V professionals achieve efficient, aesthetic results
WEST HARTFORD, Conn., June 4, 2014 – Middle Atlantic Products, a group brand of Legrand, offers a suite of Wiremold® solutions that enhance the productivity of meeting rooms through advanced cable management that is tailored for audio/video applications. These Meeting Room Solutions are especially valuable where existing space is being reconfigured to accommodate new work styles and a greater use of A/V. These products will be on display at the Middle Atlantic booth (C9325) during InfoComm 2014 and are available through the Middle Atlantic dealer network.

Legrand Expands Recall of Wiremold Under-Cabinet Power Strips Due to Electric Fire Hazard

WASHINGTON, D.C. - Consumers should stop using this product unless otherwise instructed. It is illegal to resell or attempt to resell a recalled consumer product.  This recall involves all Wiremold and Plugmold under-cabinet power and lighting strips with part number PX1001. The recalled power strips have four outlets and one fluorescent light and were manufactured from January 2011 through December 2013. From January 2011 through June 2012, the power strip came in a red package with the words “Legrand” and “Under Cabinet Power and Lighting” on the top front and “Wiremold-Series Part PX1001” on the bottom front. From July 2012 to April 2013, the power strip came in a white package with the word “Legrand” on the top front and “Plugmold Power Light,” “Under-Cabinet Power and Lighting” and “PX1001” on the bottom front. The manufacture date code is on the bottom of the recalled power strip in a circle with the year shown as "11," "12" or “13” in the center and an arrow pointing to the number representing the month. Part number PX1001, and UPC number 0 86698 00125 3, are imprinted on the bottom of the power strip. Incidents/Injuries: The firm received one report of an incident. No injuries were reported

Legrand Introduces Evolution Series Ceiling Box

Designed for conference rooms, classrooms, training facilities and more
WEST HARTFORD, Conn., April 21, 2014 – Legrand has introduced the latest in its line of high-performance wire and cable management devices – the Evolution™ Series Ceiling Box. Offered in six variations, 2' by 2' by 6" deep boxes fit above a false or permanent ceiling to provide storage for electronic audio/video and IT equipment, and to support a projector, if required. These boxes are designed for conference rooms, classrooms, training facilities, or anywhere a projector and/or A/V equipment is needed and where large racks or furniture storage are not practical.