COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

New Plugmold Multioutlet Systems Offer Enhanced USB Charging


WEST HARTFORD, Conn., November 19, 2014 Legrand has expanded its line of Plugmold® Multioutlet Systems to offer more USB charging capability. New units include all-USB options, a unit with alternating USB ports and power receptacles, and one with a single dual USB module and receptacles. These Plugmold Multioutlet Systems meet the growing demand for device charging in airport departure areas, waiting rooms, homes, and even bars – anywhere people need to charge mobile devices. All feature dual-port charging modules that share 2.4 amps of charging capacity and can charge multiple phones, tablets, or other mobile devices at the same time.

 

  • All-USB Plugmold Multioutlet Systems provide maximum charging capacity. These easy-to-install units are available in 3' and 5' lengths with 3 or 5 dual USB ports.

 

  • Alternating USB charging modules and power receptacles provide flexibility for direct USB charging, AC adapters, and plug-in appliances. Tamper-resistant receptacles prevent the insertion of foreign objects into receptacles reducing the risk of shock or electrocution. These units are available in 5' lengths only.

 

  • Single USB module and receptacles accommodate bulky AC adapters. Tamper-resistant receptacles provide safety for multi-user facilities, residential living spaces, and kitchens. These units are available in 3', 5' and 6' lengths.

 

Designed to mount easily on walls, the low-profile design is convenient to use and aesthetically pleasing.

All new Plugmold units are offered in a variety of colors and finishes, including black, ivory, white, and gray, as well as anodized aluminum and stainless steel.  Units with tamper-resistant receptacles meet 2014 NEC section 406 requirements.


 

# # #

 

 

About Legrand
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of close to $5.8 billion in 2012. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, NuVo, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819). www.legrand.us

 

Follow us on Twitter: @LegrandNA and @Wiremold.

 

 

Media contact:

Bill Graulty

(860) 679-9761

billg@mintz-hoke.com