COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand Introduces High-Capacity Furniture Feed Poke-Thru


WEST HARTFORD, Conn., February 23, 2015 – Legrand has upgraded its highly successful dual-service, furniture feed poke-thru device. The Wiremold® 4FFATC15 Series furniture feed poke-thru device is an excellent solution for feeding power, communication, and audio/video services to modular furniture systems in an open-space, above-grade environment.

With a 3/4" [19mm] opening for power and a larger 1 1/2" [38mm] opening for communication cabling, the 4FFATC15 Series furniture feed poke-thru offers more capacity for communication cabling than was previously available.

These poke-thru devices can be installed on tile, carpet, or wood covered concrete floors in both new or retrofit construction. Typical applications include commercial office buildings, financial institutions, and government facilities.

4FFATC15 Series furniture feed poke-thru device feature built-in TopGuard™ protection that prevents water, dirt, and debris from entering power and communication compartments. In addition to exceeding UL scrub water exclusion requirements for tile and carpet floors, these devices are fire rated for up to 2-hours, are suitable for use in air handling plenums, and are UL Listed and UL Fire Classified to U.S. and Canadian safety standards for tile, carpet and wood floor surfaces.

 # # #

About Legrand
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide. Innovation for a steady flow of new products with high added value and acquisitions are prime vectors for growth. Legrand reported sales of close to $5.8 billion in 2012. Legrand has a strong presence in the North American market, with a portfolio of well-known product lines that include Cablofil, Electrorack, Middle Atlantic, NuVo, On-Q, Ortronics, Pass & Seymour, Vantage, Watt Stopper and Wiremold. The company is listed on NYSE Euronext and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI and DJSI (ISIN code FR0010307819).
www.legrand.us.

Twitter: @LegrandNA and @Wiremold

Media contact:
Bill Graulty
(860) 679-9761
billg@mintz-hoke.com