COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response.
Menu
Search
Menu
RSS Feed

Legrand Enhances Evolution™ Series with more product offerings in floor box and poke-thru lines


WEST HARTFORD, Conn., June 20, 2016 Legrand, a global leader in power, light and data technologies, announces enhancements to its Evolution Series family of products with the addition of floor boxes and newly designed covers for its 6-inch and 8-inch poke-thru devices. These enhancements and additions continue to provide solutions for spaces for where power, communications and AV connectivity is needed in new or retrofit projects.

Evolution Series floor boxes are designed to work in any type of floor construction, including concrete, raised, or wood. New 4- and 5-gang versions are in addition to existing 6-, 8-, and 10-gang floor boxes.

“Our customers enjoy many of the unique features the 6-, 8-, and 10-gang floor boxes provide, but were asking for a lower capacity option,” said Mike Cole, Senior Product Manager for Legrand’s Wiremold® product line. “So, we added to our family of floor boxes by developing the new 4-and 5-gang floor boxes that all the come with the same unique features found in our existing line.”

The success of the newly released Wiremold 10-inch poke thru, as part of the Evolution Series family of products, has led to design enhancements to the 6-inch and 8-inch poke-thru covers. The 6-inch and 8-inch poke-thru’s now come with the same durable, aesthetically pleasing and easy to use cover that is found on the 10-inch poke-thru.   The heavy-duty, die-cast aluminum covers are built to withstand heavy foot traffic encountered in open spaces. Covers are manufactured with a durable, self-aligning hinge assembly and swivels open a full 180 degrees. When compared to traditional flip-top covers, the fully open cover is expected to reduce tripping incidents.

“The improved durability and ease of use with our new 10-inch poke-thru covers was met with such praise from customers that we decided to expand this design to our existing  6” and 8” Evolution poke-thru family of products,” added Cole.

Evolution Series floor boxes and poke-thru devices are UL listed. The poke-thru devices are UL fire classified for up to two hours in accordance with U.S. and Canadian safety standards. They also meet all scrub water requirements.

Evolution Series floor boxes and poke-thru devices are available at electrical distributors or through the Middle Atlantic Products dealer network.

###

 About Legrand 

Legrand is the global specialist in electrical and digital building infrastructures.  Its comprehensive offering of solutions for use in commercial, industrial and residential markets makes it a benchmark for customers worldwide.  Innovation for a steady flow of new products with high added value is a prime vector for growth, including in particular connectable products enhancing value in use. Legrand reported sales of $5.3 billion in 2015.  Legrand has a strong presence in North America, with a portfolio of well-known product lines that include C2G, Cablofil, Electrorack, Luxul, Middle Atlantic, Nuvo, On-Q, Ortronics, Pass & Seymour, Pinnacle Architectural Lighting, QMotion, Quiktron, Raritan, Vantage, Watt Stopper, and Wiremold.  Legrand is listed on Euronext Paris and is a component stock of indexes including the CAC40, FTSE4Good, MSCI World, ASPI, Corporate Oekom Rating and DJSI (ISIN code FR0010307819). www.legrand.com 

 

Media contacts:

PAT SPADAFORE | Senior Content manager PR
EMA | ERIC MOWER + ASSOCIATES
211 W. Jefferson St., Syracuse, NY 13202 
P 315.413.4360   F 315.466.2000   C 315.440.9177
pspadafore@mower.com mower.com LinkedIn Twitter