COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response. Normal ship times remain in effect for available products.
Menu
Search adorne
explore our collections

Menu
Motion Sensor Switch Auto On / Off, White
Sorry! That combination does not exist.
$42.58USD
Qty
WHERE TO BUY
ADD TO CART
Specifications
General Info
Color: White
Product Series: adorne Motion Sensor Switch
Number Of Poles: 4-Way
Style: Motion Sensor
Listing Agencies/Third Party Certifications
UL Standard: Yes
Dimensions
Depth (US): 1.85"
Height (US): 1.77"
Length (US): 2.66"
Width (US): 1.77"
Technical Information
Volts: 120
Watts: 600

Single Pole 3 Way


Ul listed logo
You Might Like
adorne 1-Gang Powder White Wall Plate
Powder White 1-Gang Wall Plate
AWP1G2PW4
(3 Reviews)
$8.88USD
adorne 1-Gang accent lgiht
Accent Nightlight, 1-Gang
AAAL1G4
(1 Reviews)
$20.98USD
adorne White Sensa Dimmer
Motion Sensor Dimmer Switch, 700W Incandescent/Halogen, White
ADSM703HW2
(2 Reviews)
$51.28USD
adorne Magnesium Timer Switch
Timer Switch, Manual-ON / Timed-OFF, Magnesium
ASTM2M2
(4 Reviews)
$52.38USD
Ratings
Rated 1 out of 5 by from Does not do what its supposed to do i recently bought this item, it is installed and turns off and on using the manual function but the motion sensor does not work. the wiring is right and it has been let with sufficient time unbothered yet it does not turm the lights on.
Date published: 2019-12-28
Rated 1 out of 5 by from This switch works irratically. When you enter the this switch turns on. Also it turns on multiple times when no one enters the room. I have replaced this switch twice in my house, and it still acts irratically. Whoever engineered this switch needs help.
Date published: 2018-12-09
Rated 1 out of 5 by from Sensor Switch Only switched to Adorne sensor for upgraded look with current sensor ( that was working fine). Could not get Adorne to work past test mode. Had to purchase another ‘on / off ‘ Adorne switch ( without sensor) to finish which worked fine. Went to website to trouble shoot and section of website was down dealing with the Adorne switch troubleshooting.
Date published: 2019-02-17
Rated 5 out of 5 by from Motion is the best in my garage I bought this motion sensor and installed it into the garage. It is the best! I light turns on as soon as I walk out in the dark and also works when I start pulling into the garage. It lights up the whole garage and that is excellent. Helps when I have my hands full.
Date published: 2018-04-04
  • y_2020, m_8, d_8, h_16
  • bvseo_bulk, prod_bvrr, vn_bulk_3.0.10
  • cp_1, bvpage1
  • co_hasreviews, tv_0, tr_4
  • loc_en_US, sid_ASOS32W4, prod, sort_[SortEntry(order=HELPFULNESS, direction=DESCENDING), SortEntry(order=POSITIVE_FEEDBACK, direction=DESCENDING), SortEntry(order=SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 47ms
  • REVIEWS, PRODUCT

I Want to know if I do install this in a garage, and let's say I'm working in the garage and switch is not in a view of motion obviously it will trigger "Off" sequence since it does not detect any motion, but my question is can it be manually switched on?

Asked by: Peter G
If you want to cover a larger area to keep the light turned on, install two of them, one in each area, wired in parallel. Either one will turn on the light.
Answered by: Mark Krisburg
Date published: 2020-07-22

Does this switch need a ground and a neutral? I have no ground and no neutral in my 1929 home. I only have a hot (load) and a return to the main breaker. I want to install this inline by breaking the the hot or return. Can this be done using this switch?

Asked by: STARGATE
This switch works poorly. I recommend you do not buy it.
Answered by: Valerie
Date published: 2020-04-20

Will this work with a bathroom exhaust fan? If not, which sensor should I use for that. 

Asked by: bcohler
Yes, as long as your bath fan does not exceed the 1/6HP rating for the sensor.
Answered by: Legrand Technical Support
Date published: 2019-06-24

Does it work with LED/CFL 450W?

Asked by: cecilia
It is designed to handle Incandescent or CFL/LED lamp: 0-600 Watt's.
Answered by: Legrand Technical Support
Date published: 2020-05-28

Is it compatible with 0-10V LED drivers?

Asked by: cecilia
It is not compatible with 0-10V drivers.
Answered by: Legrand Technical Support
Date published: 2019-02-13

I have this in the entrance to my bathroom and it works fine when I enter.  However it always turns off before I am done and I have to leave in the dark.  Is there a way to adjust how long the light stays on before it turns off?

Asked by: MikeG
I heard from Legrand support team and learned I can adjust the delay time using the trimpot. The range is 30 seconds  up to 30 minutes. You can also set the switch so it does not turn on in daylight. These functions are explained in the installation instructions.
Answered by: MikeG
Date published: 2019-05-15

Can this be combined with a Wi-Fi Master Switch (ASTH155RMW1) to control a single light from two locations (replacing an existing 3-way switch setup)? i.e. to allow motion-activation of the light AND allow control of the light through Wi-Fi?

Asked by: devc
The answer would be no since the dimmer can't communicate via Wi-Fi with the master you mentioned.
Answered by: Legrand Techincal Support
Date published: 2019-03-20

After testing the switch by putting the trimpot to minimum, the switch now reverts to a shutoff delay of 5 mins even though I have the trimpot moved to the lowest setting before entering test mode again. How do I get lowest delay set?

Asked by: Jason
You would want to turn the trimpot all the way counter clockwise. That will put the time delay to the 5 second time delay.
Answered by: Legrand Technical Support
Date published: 2018-07-05
  • y_2020, m_8, d_9, h_16CST
  • bvseo_bulk, prod_bvqa, vn_bulk_3.0.10
  • cp_1, bvpage1
  • co_hasquestionsanswers, tq_10
  • loc_en_US, sid_ASOS32W4, prod, sort_[SortEntry(order=LAST_APPROVED_ANSWER_SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 32ms
  • QUESTIONS, PRODUCT
  • bvseo-msg: The getReviews method is only supported when schema.org is configured for structured markup. Please submit a support ticket at spark.bazaarvoice.com to have your Bazaarvoice configuration updated to use schema.org for structured markup.;

Chat Is Currently Offline

Leave a message here to request a call back from our customer support team.



Submit