COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response. Normal ship times remain in effect for available products.
Menu
Search adorne
explore our collections

Menu
Pop-Out™ Outlet, 15A, 1-Gang, White
Sorry! That combination does not exist.
$45.48USD
Qty
WHERE TO BUY
ADD TO CART
Specifications
General Info
Color: White
Product Series: adorne Pop-Out Outlet
Number Of Wires: 3
Style: Pop-Out
Listing Agencies/Third Party Certifications
UL Standard: Yes
Dimensions
Height (US): 1.77"
Length (US): 1.77"
Width (US): 1.77"
Technical Information
Amps: 15A
Mounting: USA Electrical Wiring Box / adorne Mounting Plate
Volts: 125
Number Of Receptacles: 3
Ul listed logo
You Might Like
adorne 1-Gang Powder White Wall Plate
Powder White 1-Gang Wall Plate
AWP1G2PW4
(3 Reviews)
$8.88USD
adorne 1-Gang accent lgiht
Accent Nightlight, 1-Gang
AAAL1G4
(1 Reviews)
$20.98USD
adorne White Half Size USB Outlet
USB Outlet, Half-Size, White
ARUSBW4
(6 Reviews)
$24.28USD
adorne White Tamper Resistant Outlet
Outlet, 15A, White
ARTR152W4
(11 Reviews)
$4.48USD
Ratings
Rated 2 out of 5 by from Nice idea... but could be better I just got them installed and I have to say, I am a little disappointed. I was expecting this to be more flushed and seamless with our island, but after installing it, it actually is not flush due to this additional backing and the contrast of the black backing calls out attention to it. I like the idea of the plug being hidden, but thought it was designed to be more flush (flat) against the surface so it doesn't call attention to it. If that is what you are looking for, i would make sure you are ok with the thickness before making the purchase.
Date published: 2019-12-08
Rated 4 out of 5 by from Neat Idea, Nice lines Once it was installed I really liked the look of the pop out outlet. THe installation was a tad trickier than the usual standard outlet which is to be expected but I youtubed it and got through it without an electrician. The lines of the outlet and cover are great and the pop out seemes to work well. My only critique is that my different sized plugs don't all work with it. I needed to plug in an extension cord to run a shop vac where a leak had happened and it didn't pop out far enough to accomodate.
Date published: 2018-10-31
Rated 5 out of 5 by from A Win-Win: Sophisticated Design and Three Plugs The Pop-Out outlet provides a modern addition to your walls, avoiding those unsightly traditional outlets. The outlet features an additional plug (three total) over traditional outlets and with the simple push before/after use, the outlet pops-out/disappears into the wall. Thus far, we have had no issues and look forward to installing more throughout the house. We have this outlet at the far side of our kitchen where we keep/charge our electronics and smarthome base. Previously, we were maxxed out on the plugs in the outlet, and now we have an additional plug that we have been using. I wonder how we ever functioned without a third plug. Installation time was minimal, about 10 minutes, which is typical of an outlet change. Prior to install, make sure you have a deep electrical box so you can properly fit the outlet and its wires. One word of caution: the outlet is only meant for indoor wall surfaces, so if you are hoping to install on a horizontal work surface, look elsewhere. Also, for those who want your outlet childproofed, I would look elsewhere if you plan to install these below counter height, as there does not appear to be a way to childproof this outlet. As my (past childproof age) children are fascinated by this outlet, I imagine little kids would be even more fascinated by the popping action. I do not believe you can go wrong installing these outlets in your home. They will supply an additional plug at every outlet, as well as provide an updated and stylish complement to any room they adorn.
Date published: 2018-10-29
Rated 5 out of 5 by from Fantastic Look and Functionality I bought two of these outlets to be installed on my kitchen island and they became a decoration element. It perfectly complement our contemporary, clean style and it is great to see them “disappear” when not in use. Installation is a breeze. It is a bit pricey, but for those concerned about look and style, without sacrificing functionality is a must.
Date published: 2019-07-16
Rated 5 out of 5 by from Finally! An outlet with style and versatility! I love clean lines and nothing irritates me more than trying to "cover up" electrical outlets that are not in use. I also dislike plugs that stick out of outlets an inch or so. Furniture cannot be put up against the wall without making room for the bulky plugs. I've been buying flat plug extension cords but then I have the long cords to deal with. I love the Pop-Out Outlet! The installation was simple and the simplistic style fits in so well with backsplashes and walls. When needed,, simple push the square in the middle of the plate and the outlets "pop" out. No need to lose any more room to accommodate the plugs and cords that are plugged into normal outlets, other than the space required for the popped out outlet. Can't wait to install more throughout the house!
Date published: 2019-01-08
  • y_2020, m_8, d_9, h_16
  • bvseo_bulk, prod_bvrr, vn_bulk_3.0.10
  • cp_1, bvpage1
  • co_hasreviews, tv_0, tr_15
  • loc_en_US, sid_ARPTR151GW2, prod, sort_[SortEntry(order=HELPFULNESS, direction=DESCENDING), SortEntry(order=POSITIVE_FEEDBACK, direction=DESCENDING), SortEntry(order=SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 16ms
  • REVIEWS, PRODUCT

My outlet won't stay closed. I'd there a way to fix it?

Asked by: Tiffcincy
Please contact Technical Support for assistance with this: adorne products 1.800.223.4185 opt 3 Mon - Fri: 8am - 6pm EST (excluding holidays) Email Us - tech.support@legrand.us
Answered by: Legrand Technical Support
Date published: 2020-07-22

My duplex pop out outlet came with the outlets on the top and bottom. Any way to switch them to the sides?

Asked by: Sparky 2020
Yes, you can rotate them as you like
Answered by: Home improver 2019
Date published: 2020-01-30

I want to install a pop-out with a 1-gang wall plate. Can I choose to orient the wall plate as either portrait (tall) or landscape (wide)? Or is it only possible to have portrait orientation? Or, does it depend on the orientation of the box behind?

Asked by: Mary
The Popout outlet can function either in portrait or landscape orientation but it will depend on the position of the electrical box. Keep in mind that if you do mount it horizontal, when you apply the adorne wallplate, the Legrand stamp on the face will be out of place because it is designed for vertical installation.
Answered by: Legrand Technical Support
Date published: 2020-01-21

I have a "niche" within a wall with a plug on its surface (sitting on top) - I read it could not be installed on a horizontal surface: Is it not advised / no possible? What is the risk?

Asked by: VinceP
The Popout receptacle is UL listed for wall mount only because of the possibility of moisture or liquid getting into the electrical device. CAUTION: Do not install into a countertop or similar work surface. For use in indoor wall surfaces only.
Answered by: Legrand Technical Support
Date published: 2019-11-15

do you have for EU 220v 240v

Asked by: azores
The Popout outlets are available for 120V only.
Answered by: Legrand Technical Support
Date published: 2019-10-25

How is this child proof if you just push/tap to have it pop out to use?

Asked by: Sissie
The Popout outlet, as well as all of the adorne receptacles contain a tamper-resistant built-in shutter system that allows plugs to be inserted when equal pressure is applied simultaneously to both sides of the receptacle. Tamper-resistant outlets reduce the risk of electrical injuries.
Answered by: Legrand Technical Support
Date published: 2020-01-13

Is the pop-out outlet weather proof?

Asked by: James
It is not weather proof.  
Answered by: Phil
Date published: 2019-10-29

What is the minimum depth requirement for the installation of this device?

Asked by: James
The pop out outlet needs a 3.5" deep box.
Answered by: Legrand Techincal Support
Date published: 2019-10-24
  • y_2020, m_8, d_9, h_16CST
  • bvseo_bulk, prod_bvqa, vn_bulk_3.0.10
  • cp_1, bvpage1
  • co_hasquestionsanswers, tq_24
  • loc_en_US, sid_ARPTR151GW2, prod, sort_[SortEntry(order=LAST_APPROVED_ANSWER_SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 15ms
  • QUESTIONS, PRODUCT
  • bvseo-msg: The getReviews method is only supported when schema.org is configured for structured markup. Please submit a support ticket at spark.bazaarvoice.com to have your Bazaarvoice configuration updated to use schema.org for structured markup.;

Chat Is Currently Offline

Leave a message here to request a call back from our customer support team.



Submit