Menu
Search adorne
explore our collections

Menu
sofTap™ Switch, White
Sorry! That combination does not exist.
$44.28USD
Qty
WHERE TO BUY
ADD TO CART
Specifications
General Info
Color: White
Product Series: adorne sofTap Switch
Number Of Poles: Single Pole/3-Way
Style: sofTap
Listing Agencies/Third Party Certifications
UL Standard: Yes
Dimensions
Depth (US): 1.63"
Length (US): 2.66"
Width (US): 1.77"
Technical Information
Amps: 15A
Volts: 120
Ul listed logo
You Might Like
adorne 1-Gang Satin Nickel Wall Plate
Satin Nickel 1-Gang Wall Plate
AWC1G2SN4
(0 Reviews)
$38.28USD
adorne 1-Gang accent lgiht
Accent Nightlight, 1-Gang
AAAL1G4
(0 Reviews)
$20.98USD
adorne White SofTap Switch Tru-Universal Award Winner
sofTap™ Dimmer Switch, 700W Tru-Universal, White
ADTP703TUW4
(19 Reviews)
$60.98USD
adorne White SofTap Switch
sofTap™ Wi-Fi Ready Master Switch, White
ASTP155RMW1
(3 Reviews)
$74.98USD
Ratings
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 44ms
  • REVIEWS, PRODUCT
  • bvseo-msg: The resource to the URL or file is currently unavailable.;

I have successfully installed these switched to one way and 3-pole lights but I am having trouble with one switch of mine, a softap to an insinkerator on/off switch with just a hot and neutral wire wired correctly, however it will not shut off. Help!

Asked by: Sara
I had this issue. Turns out the ground is required for the switch shutoff. You need to wire the ground.
Answered by: IvanJ
Date published: 2019-12-28

Universal Soft tab dimmer 3 way install, installed dimmer and working however, when I try to connect the other soft tap switch following instructions, switch does not work, help please. 

Asked by: VicNC
First I would verify that the Softap switch is snapped into the metal mounting frame that has good Ground connection seeing the electronic adorne switch need that to work. Also, When using True Universal Dimmer in a 3 way application, with an electronic switch (Soft Tap, Touch, or Wave), the HOT wire MUST be connected to the electronic switch, and the dimmer MUST be connected to the load. Reversing this wiring (HOT to Dimmer and LOAD to Switch ) will cause the switch to stop functioning. The switch requires 120 VAC to operate. When the voltage to the switch is lowered by using the dimmer, the electronics in the switch stop functioning. This only applies when using an electronic switch. A standard switch (Paddle, Push and Whisper, for example) is not effected.
Answered by: Legrand Technical Support
Date published: 2019-12-19

I’m trying to use the softap on/off switch (not the dimmer) to supply power to a Minka Aire fan. The switch will not turn off the power. I’ve tried the switch w/o the luminaire wired into the switch and it still will not turn off. Any suggestions?

Asked by: Granddude
I would check the Ground connection to the Softap switch and it does need to be snapped into the metal mounting frame to function. The electronic switches in the adorne line have to have to be Grounded to work.
Answered by: Legrand Technical Support
Date published: 2019-10-03

Are these switches Philips Hue compatible? If I use these to turn off the lights, can I still use Alexa/hue app to turn them back on?

Asked by: Smart home newbie
Does it still work if I used the switch to turn off the lights and then try to turn the bulbs on using the Philips Hue APP? My understanding is that the Philips Hue bulbs do not work if the lights are switched off manually by using a wall switch. I'm not sure if this type of switch is an exception as there is no on/off flip.
Answered by: Smart home newbie
Date published: 2019-05-30

After completing install the switch does not turn off. Existing wires where installed per instructions. The locator light wires are connected to the 3-WAY terminal and in the same hole as power at the 1-POle terminal. Help please

Asked by: UHredneck
If you're using the switch for an LED, it won't work right, since the leakage current powering the locator light is enough to light the load. Also, the written wiring instructions supplied for the locator light are for installing as a three-way switch. They don't tell you that in the instructions, but the wires for the locator light need to be connected differently if you are using the switch in a one-pole configuration. If you're able to navigate to the page on this website for the illuminator (locator light), you'll see in the question section that they give the wiring requirement for a one-pole installation as hot and one-pole (instead of one-pole and 3-way, as in the written instructions supplied with the product).
Answered by: Another frustrated user
Date published: 2019-04-28

Is the light in the middle of the SoftTap switch as bright as the light on the Touch Dimmer?

Asked by: Alayne
Hello, The LED locator light in both switches is the same. Hope this helps, Have a great day.
Answered by: Legrand Techincal Support
Date published: 2019-01-05

Can this switch be used to turn on a fan?

Asked by: Harrison
Hello, Yes , this switch can be used for a fan. Hope this helps, Have a great day.
Answered by: Legrand Techincal Support
Date published: 2018-12-15

Can the softap dimmer be used in a 3way with the ASPD1532W4?

Asked by: Ignite
The Softap SP/3W dimmers can be used with the SP/3W Softap switch. When using an electronic switch (Soft Tap, Touch, or Wave), the HOT wire MUST be connected to the electronic switch, and the dimmer MUST be connected to the load.
Answered by: Legrand Technical Support
Date published: 2018-11-11
  • y_2020, m_1, d_24, h_15CST
  • bvseo_bulk, prod_bvqa, vn_bulk_3.0.4
  • cp_1, bvpage1
  • co_hasquestionsanswers, tq_12
  • loc_en_US, sid_ASTP1532W4, prod, sort_[SortEntry(order=LAST_APPROVED_ANSWER_SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 40ms
  • QUESTIONS, PRODUCT
  • bvseo-msg: The getReviews method is only supported when schema.org is configured for structured markup. Please submit a support ticket at spark.bazaarvoice.com to have your Bazaarvoice configuration updated to use schema.org for structured markup.;

Chat Is Currently Offline

Leave a message here to request a call back from our customer support team.



Submit