COVID-19 Update
A message from John Selldorff on the COVID-19 virus and what LNCA is doing in response. Normal ship times remain in effect for available products.
Menu
Search adorne
explore our collections

Menu
Accent Nightlight, 1-Gang
You Might Like
adorne Locator Status Light
Locator Status Light
AALSL6
(0 Reviews)
$4.38USD
Flashlight
Portable Nightlight / Flashlight
AARNL2
(1 Reviews)
$50.18USD
adorne White 20 amp Paddle Switch
Paddle™ Switch, 15A, White
ASPD1532W4
(14 Reviews)
$5.68USD
adorne White Paddle Dimmer
Paddle™ Dimmer Switch, 700W Incandescent/Halogen, White
ADPD703HW4
(2 Reviews)
$36.68USD
Ratings
Rated 1 out of 5 by from Poor functionality - Comes on at random! The adorns nightlight sounds like a cool feature to add to a switch- granted it works as advertised. We’ve found that it will come on during the day at random due to changes in ambient lighting, and even at night without changes in ambient light in our toddlers room- waking him up at 2 am (look at time stamp on this review) and it keeps coming on at full brightness setting. Clearly very faulty sensor. Sadly we might need to uninstall this feature. Step up your game Legrand!!
Date published: 2020-02-25
  • y_2020, m_8, d_8, h_16
  • bvseo_bulk, prod_bvrr, vn_bulk_3.0.10
  • cp_1, bvpage1
  • co_hasreviews, tv_0, tr_1
  • loc_en_US, sid_AAAL1G4, prod, sort_[SortEntry(order=HELPFULNESS, direction=DESCENDING), SortEntry(order=POSITIVE_FEEDBACK, direction=DESCENDING), SortEntry(order=SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 31ms
  • REVIEWS, PRODUCT

Does this nightlight work with a Radiant wall plate / receptacle?

Asked by: VotD
The light is so week, does not help.
Answered by: John
Date published: 2020-05-20

Does the accent nightlight require a different gang plate or frame?  

Asked by: Stef
The Accent Nightlight will work with any adorne(1-4 Gang) wallplate.
Answered by: Legrand Technical Support
Date published: 2020-04-02

Will the AAALG1G4 Nightlight work with a 3-way switch in a 3 wire application in conduit? What should the neutral wire be connected to?

Asked by: Grandpa Russ
The Accent Nightlight can only be install on the LINE side of a 3way and the white wire needs to be connected to a white Neutral wire.
Answered by: Legrand Technical Support
Date published: 2020-02-14

1. how is this different from AANLM24, which is also night light 2. will this and AANLM24 work with 1 Gang+ plate? thanks in advance for your answers

Asked by: txman
1. The AANLM24 is a full size nightlight that takes the place of a device in the wallplate, where the AAAL1G4 is the Accent nightlight that gets installed behind the wallplate along with your switch, dimmer, or outlet, etc... 2. You could potentially put the AANLM24 and the AAAL2G4 together in a one gang box using the standard 1 gang wallplate(not the Plus size).
Answered by: Legrand Technical Support
Date published: 2019-12-16

Do these nightlights have sensors to automatically turn them off in daylight ?

Asked by: narain
Yes they do. Whether day light or full lighting is turned on in the room.
Answered by: JG_Upgrades
Date published: 2019-11-21

I installed less than an inch from a counter top. When ambient light is on the accent light just blinks. When the ambient light is off the accent light scrolls through the brightness settings continually. Is there a way to override?

Asked by: Justin
Sounds like something is covering the sensor on the bottim that lets you turn it off and on and go through lights brightness. May want to pull the wall plate off and look to see what may be blocking the sensor. I've had a similar issue but, I believe my issue is due to the wall box being a tight fit. The issue seems to be intermittent depending on objects that may be put close to it and cause a shadow making the sensor think a finger is being put there to turn on/off the light or adjust the brightness.
Answered by: JG_Upgrades
Date published: 2020-04-09

Will the accent light attach to an accent outlet (power plug), in addition to the switches?

Asked by: esdee
Good Morning, Yes, they will work with all of our outlets except the PopOut. Hope this helps!
Answered by: Tech Support
Date published: 2019-04-09

I ONLY HAVE THREE WIRES (INCLUDING GROUND) - IS THERE ANY WAY TO STILL CONNECT THE ACCENT LIGHT...

Asked by: ADAM
Thank you for your question regarding the adorne Accent Nightlight(Model # AAAL1G4). To install the Accent Nightlight is only requires a Hot & Neutral connection to function.
Answered by: Legrand Technical Support
Date published: 2020-04-09
  • y_2020, m_8, d_9, h_16CST
  • bvseo_bulk, prod_bvqa, vn_bulk_3.0.10
  • cp_1, bvpage1
  • co_hasquestionsanswers, tq_9
  • loc_en_US, sid_AAAL1G4, prod, sort_[SortEntry(order=LAST_APPROVED_ANSWER_SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 16ms
  • QUESTIONS, PRODUCT
  • bvseo-msg: The getReviews method is only supported when schema.org is configured for structured markup. Please submit a support ticket at spark.bazaarvoice.com to have your Bazaarvoice configuration updated to use schema.org for structured markup.;

Chat Is Currently Offline

Leave a message here to request a call back from our customer support team.



Submit