Menu
Search adorne
explore our collections

Menu
Wave™ Switch, White
Sorry! That combination does not exist.
$58.28USD
Qty
WHERE TO BUY
ADD TO CART
Specifications
General Info
Color: White
Product Series: adorne Wave Switch
Number Of Poles: Single Pole/3-Way
Style: Wave
Listing Agencies/Third Party Certifications
UL Standard: Yes
Dimensions
Depth (US): 1.71"
Length (US): 2.66"
Width (US): 1.77"
Technical Information
Amps: 15A
Volts: 120
Ul listed logo
You Might Like
adorne 1-Gang Powder White Wall Plate
Powder White 1-Gang Wall Plate
AWP1G2PW4
(3 Reviews)
$8.88USD
adorne 1-Gang accent lgiht
Accent Nightlight, 1-Gang
AAAL1G4
(0 Reviews)
$20.98USD
Ratings
Rated 5 out of 5 by from Stress free I bought the Wave switch because I have OCD which causes me to not like to touch things only if they are disinfected which causes extra work for me on my daily routine unfortunately. This has helped cut back a few minutes to free up some time in my day for me. I wish the company made a two and three toggle switch waves for the living room and kitchen lights. If and when they do I will definitely purchase them. Thank you Adorne for making my life a little easier
Date published: 2018-10-25
Rated 5 out of 5 by from works great Love it just remodeled by bathroom and every switch and outlet is legrand
Date published: 2018-04-04
Rated 5 out of 5 by from Great Upgrade To My Modern Home The Wave Switch works perfectly and looks even better. It gives off a very modern and high tech feeling. Being able to adjust the distance your hand needs to be to trip the switch is a great feature. I bought the Wave Switch to be used in my bathroom. I thought it would be a great to reduce the spread of germs. It's one less thing that has to be touched. Only advice I have is to be sure not to hang a hand towel in front of it as that will trip the sensor.
Date published: 2018-11-15
Rated 5 out of 5 by from Works well Easy to install, works as it should. Added locater light but is difficult to see at night,needs a larger opening. Great style
Date published: 2018-08-06
  • y_2020, m_1, d_24, h_15
  • bvseo_bulk, prod_bvrr, vn_bulk_3.0.4
  • cp_1, bvpage1
  • co_hasreviews, tv_0, tr_4
  • loc_en_US, sid_ASWV1532W2, prod, sort_[SortEntry(order=HELPFULNESS, direction=DESCENDING), SortEntry(order=POSITIVE_FEEDBACK, direction=DESCENDING), SortEntry(order=SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 7ms
  • REVIEWS, PRODUCT

Will the wave switch work with LED can lights lighting a staircase? What is the maximum distance adjustment for the wave to work?

Asked by: Eweneek1
The Wave switch will work on any type of light load and the sensitivity range is 1 to 6 inches in front of the switch.
Answered by: Legrand Technical Support
Date published: 2019-12-16

Will the wave outlet work for a sink garbage disposal?

Asked by: Jen72
The adorne Wave switch can control a motor as long as it does not exceed it's 1/2HP rating.
Answered by: Legrand Technical Support
Date published: 2019-12-02

I have 2 hot 2 neutral and 2 ground in the existing box. The 2 hot in the hot portal and 2 neutral in the one pole portal??

Asked by: Breel55
Typically, if you have two black wires and two white wires you would connect the Hot black wire to the HOT terminal and the other black wire(LOAD) would get connected to the 1POLE terminal and your white Neutral wires get bundled together with a wire nut and put to the back of your electrical box. The Wave switch does not require a Neutral connection. Your Ground wires can be connected together to the Green wire on the mounting frame. adorne products 1.800.223.4185 opt 3 Mon - Fri: 8am - 8pm EST (excluding holidays) Email Us - tech.support@legrand.us
Answered by: Legrand Technical Support
Date published: 2019-11-26

How do I fix the light remaining in "dim" mode? This is a wave switch that doesn't have dimmer. I grounded as instructed. Thanks

Asked by: Dhyana
If you are using the Locator Status Light and controlling LED's with the Wave switch, it may cause the low wattage LED's to remain on slightly. Make sure you have the Locator leads connected to HOT and 1POLE terminals for a single pole application
Answered by: Legrand Technical Support
Date published: 2019-09-24

Does this switch come with the locator light preinstalled or is that separate?

Asked by: JPenzo
The Wave switch will come with the Locator Light in the package and you have the option to install or not.
Answered by: Legrand Technical Support
Date published: 2019-09-05

HI Legrand, is there any way to have it working on 220v?

Asked by: Ernie
The adorne Wave switch is rated for 120V circuit only.
Answered by: Legrand Technical Support
Date published: 2019-08-22

Is this product wifi ready ?

Asked by: Bhensley65
This is a line voltage motion vacancy sensor which is not wi-fi ready.
Answered by: Legrand Technical Support
Date published: 2019-09-04

Hello guys. I bought Adorne Wave Switch Interruptor and installed it as manual recommended but it doesn’t work. What might be is wrong? Thank  Michael 

Asked by: Mike
The Wave switch is an electronic switch so it does require a Ground to function. Make sure it is snapped into the metal mounting frame before testing and that is has a solid Ground connection.
Answered by: Legrand Technical Support
Date published: 2019-04-16
  • y_2020, m_1, d_24, h_15CST
  • bvseo_bulk, prod_bvqa, vn_bulk_3.0.4
  • cp_1, bvpage1
  • co_hasquestionsanswers, tq_13
  • loc_en_US, sid_ASWV1532W2, prod, sort_[SortEntry(order=LAST_APPROVED_ANSWER_SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 8ms
  • QUESTIONS, PRODUCT
  • bvseo-msg: The getReviews method is only supported when schema.org is configured for structured markup. Please submit a support ticket at spark.bazaarvoice.com to have your Bazaarvoice configuration updated to use schema.org for structured markup.;

Chat Is Currently Offline

Leave a message here to request a call back from our customer support team.



Submit