Menu
Search adorne
explore our collections

Menu
sofTap™ Wi-Fi Ready Master Dimmer, Incandescent / Halogen, White
Sorry! That combination does not exist.
$111.18USD
Qty
WHERE TO BUY
ADD TO CART
Specifications
General Info
Color: White
Product Series: adorne sofTap Dimmer
Type: Incandescent/Halogen
Number Of Poles: 4-Way
Style: sofTap
Listing Agencies/Third Party Certifications
cULus: Yes
FCC Standard: Yes
UL Listing No: UL 1472
UL Standard: Yes
UN SPSC: 39122206
Dimensions
Depth (US): 1.79"
Height (US): 4.185"
Length (US): 4.20"
Width (US): 1.77"
Product Weight (US): 0.32 pounds
Technical Information
AC Voltage Output: 120VAC
Frequency: 900 MHz (RF)
Humidity: 0-80% relative humidity, noncondensing
Load: Incandescent, Halogen
Material: FR4(PCB)
Mounting: USA Electrical Wiring Box / adorne Mounting Plate
Operating Temperature (Celsius): 0°C to 50°C
Product Fits Into: Wall
Storage Temperature: 32°F to 122°F
Watts: 600

Works With Amazon Alexa

Works With The Google Assistant

Whole HouseIncandescent/HalogenUl listed logo

You Might Like
adorne White SofTap Dimmer
sofTap™ Wi-Fi Ready Remote Dimmer, White
ADTPRRW1
(0 Reviews)
$70.68USD
adorne White SofTap Switch
sofTap™ Wi-Fi Ready Master Switch, White
ASTP155RMW1
(3 Reviews)
$74.98USD
Wi-Fi Ready Outlet, White
Wi-Fi Ready Outlet, White
ARPS15RF2W4
(0 Reviews)
$36.68USD
adorne Hub and WiFI Devices
The Hub
LC7001
(7 Reviews)
$156.98USD
Ratings
Rated 5 out of 5 by from Review of sofTap Wi-Fi Ready Master Dimmer This is a replacement switch for the standard electronic dimmer switch. I recently added several of the wi-fi switches, all masters, to control several outside lights as well as a towel warmer. All have worked well and then I decided to add one more wi-fi switch which is the subject of this brief review. Instillation was not difficult and once you understand how to press in the 4 compressible snaps then exchanging one switch for another is fairly routine. The one caveat that I have found is I had several paddle switches and I was completely incapable of removing these particular switches.. I would advise not using these at all especially now since Legrand Adorne has added a mechanical push switch that is identical to the basic electronic switch. I needed the paddle switch due to electrical wiring issues that could not be resolved unless spending a lot of unnecessary money. The paddle switch resolved this problem but did not match my other electronic ones but now this problem has been resolved. These newer puch mechanical switches are like all the others, except for the paddle switches, easy to install or remove. The 4 way paddle switch has yet to be replaced with a mechanical push switch but I am hoping for this in the future. Once I turned off the electricity to the switch area, the old dimmer switch was removed without difficulty and the new wi-fi dimmer switch was installed. Then the programming started and once again I needed to call in for technical help with this issue. I have pretty good mechanical skills but the programming portion seems to escape my skill sets but luckily there are good people at Legrand Adorne for technical help. They have all proven to be patient, kind and understanding. I am sure that there are many house repair warriors such as myself but help is there so do not struggle with this. I did find one issue that has been resolved by programming the dimmer switch at the level you want. If it is not to your satisfaction, you do not need to call but wait until the program time turns on the wi-fi dimmer and then go to that particular switch in the phone app to increase or decrease the intensity of the light being controlled. Thank goodness for this little nugget. Overall, the cost, time and instillation was worth the effort. Legrand Adorne will back up their product and replace any switch that goes bad. Thank goodness there are still companies that stand by their products.
Date published: 2018-11-07
  • y_2020, m_1, d_23, h_18
  • bvseo_bulk, prod_bvrr, vn_bulk_3.0.4
  • cp_1, bvpage1
  • co_hasreviews, tv_0, tr_1
  • loc_en_US, sid_ADTP600RMHW1, prod, sort_[SortEntry(order=HELPFULNESS, direction=DESCENDING), SortEntry(order=POSITIVE_FEEDBACK, direction=DESCENDING), SortEntry(order=SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 60ms
  • REVIEWS, PRODUCT

Can I pair the Wifi switches directly to Amazon Alexa without the hub?

Asked by: mando
The LC7001 hub is required to work with Amazon Alexa.
Answered by: Legrand Technical Support
Date published: 2019-05-20

Do o need a hub to make this work With my WiFi and Elexa 

Asked by: Andy
Yes You do need the Hub (model LC7001) to get the Adorne WiFi ready products and Amazon Alexa. You do not need the Hub unless You care to use our Lighting control app or Amazon Alexa.
Answered by: Legrand Technical Support
Date published: 2019-01-28
  • y_2020, m_1, d_24, h_14CST
  • bvseo_bulk, prod_bvqa, vn_bulk_3.0.4
  • cp_1, bvpage1
  • co_hasquestionsanswers, tq_2
  • loc_en_US, sid_ADTP600RMHW1, prod, sort_[SortEntry(order=LAST_APPROVED_ANSWER_SUBMISSION_TIME, direction=DESCENDING)]
  • clientName_legrand
  • bvseo_sdk, net_sdk, 3.2.0.0
  • CLOUD, getReviews, 240ms
  • QUESTIONS, PRODUCT
  • bvseo-msg: The getReviews method is only supported when schema.org is configured for structured markup. Please submit a support ticket at spark.bazaarvoice.com to have your Bazaarvoice configuration updated to use schema.org for structured markup.;

Chat Is Currently Offline

Leave a message here to request a call back from our customer support team.



Submit