Menu
Search
Menu

Power Cables

The installation of power cabling systems relies on high quality cable supports.
CABLOFIL® takes this further, by offering a strong, fast, safe, clean and ventilated system.

 

Numerous References
Armoured, singles or twin&earth cables are the ones used most frequently in an electrical installation. They carry the power required to run electrical installations.  The choice of a power cable is based mainly on two criteria:

  • Mechanical Performance:  tension, fire rating, temperature performance, chemical resistance, shock and vibration resistance, etc.
  • Electrical Performance:  AC or DC, very low, low, medium, high or very high voltage, single-phase, or three-phase, etc. 

Solutions for all applications encountered in the electrical world can be found by combining these characteristics.  There are numerous cable references.



The Cablofil® Solution

Mechanical Performance

Cablofil® was subjected to a series of mechanical tests.  Each reference is able to support power cables.  The load tables shown in the catalogues can be used to select the most suitable reference.

All Cablofil® fittings including bends, tees, risers and sets are created to suit the installation on site while maintaining the bend radius of the cables.

Maintenance

Its open structure makes it easy to inspect the cable installation which simplifies any maintenance work that may be required.

Safety
In some installations it may be necessary to improve the safety of people and/or property.  A sufficiently large protection conductor may be used.  Cablofil® includes suitable accessories (see Earth Network).

Cleanliness
Retention of dust, ingression of bacteria and any debris obstructing the cable path are greatly reduced due to the open mesh construction of Cablofil®.

 

Testing

Ventilation of Cables
By improving the heat dissipation of power cables, substantial savings can be made on the installation and operation costs.  The open structure of Cablofil® maximizes ventilation.

 

The performance level of the cable depends on its electrical resistance.  This is proportional to the resistivity, which is in turn proportional to the temperature.  When the temperature rises, the cable resistance increases and the cable performance drops.

When electric current flows through the cable, the temperature of the central copper or aluminium conductor increases up to an operating temperature of about 70°C to 80°C.

Heat given off by the cable due to the Joule effect poses no problem in free air.  In a confined space, however, such as inside a closed cable tray or trunking, the cable will heat up and its performance will drop therefore less current will be carried.

Studies have shown that excessive cable temperature wastes considerable energy.

The resistivity of copper varies with temperature.

 
 

There are two possible solutions

A high cost solution would be to increase the cable cross-sections.
A low cost solution is to ventilate the system by installing the cables in Cablofil®.

Cablofil® is in fact the nearest thing to a cable in free air as it represents only 10% solid surface area, and in many cases is considered as such by standard IEC 60 364 standard. (NFPA 79)

Using an unventilated, or only slightly ventilated, installation method with some configurations (several power cables running in the cable tray) require the use of cables of cross-section 1.5 to 2 times larger than with Cablofil®.

 

 
 

A technical and financial advantage

The performance levels of cables supported by Cablofil® are therefore optimized, resulting in significant cost-savings :

  • Optimization of the cross-section and therefore the cost of the cable.
  • Reduction of the installation time and therefore the cost of labour.
  • Reduction of the heating effect and therefore the energy consumption.