Type
Value that Specifically Names the Type/the Application Value of the Closest Piece of Equipment/the Designated Type of Construction/the Generic Type/the Manufacturer Type Designation/the Specific Function/the Type of Application
Product Certifications
Trust in quality and compliance. Use this filter to find products that have undergone thorough testing and evaluation to ensure they meet the quality and safety standards for a wide range of certifications.
Standard
The industrial standard(s) to which a device is manufactured, operated, or tested.
Cable Specification
The Description of the Conductor Explicitly Stating the Design Criteria of the Conductors
Base Type
Style or Type of the Foundational Ingredient of Something.
Connector
A Device that Establishes a Connection Between Two or More Units.
Number of Receptacles
The Number of Electrical Wall Outlets Designed for Use with a Plug
Cable Entry
The Type/Specification of the Access Points Where the Cables are Made to Enter or Exit.
Is the Device Prewired?
Denotes whether a product comes prewired for quicker installation.
Frequency Band
A Continuous Group, or Range, of Frequencies with an Upper Limit and a Lower Limit
Has External Power Supply
External component that supplies power to an electrical circuit
Sensor Type
The Device that Receives a Signal or Stimulus (As Heat or Pressure or Light or Motion Etc.) and Responds to it in a Distinctive Manner
Amperage
Maximum electrical current the conductor or device can carry before sustaining immediate or progressive deterioration
Installation Location
Where a Device is or is to be Installed
Load
The Maximum Amount of Power Which the item can withstand or Operate without any performance Loss
Mounting
Something that Serves as a Support, Setting, or Backing for the item
Connector Type
The Type of Connectors / Terminals that Tool can Crimp to Wire or Cable
NEMA Rating
National Electrical Manufacturers Association Ratings are Standards that are Useful in Defining the Types of Environments in Which an Electrical Enclosure can be Used
Maximum Product Width
The maximum measurable width of the product.
Lamp Length
The Type of Device Designed to Produce Electromagnetic Radiation in the form of Light, Heat, Ultraviolet Energy, or a Combination of the Three.
Contact Rating
The Voltage, Current, and Power Capacities of Relay Contacts Under Specified Environmental Conditions
Frequency Range
Refers to the range of signal frequencies a product can support, which affects compatibility and performance in audio, video, and data transmission applications.
Cable Type
The Type of a Assembly of one or More Insulated Conductors, or Optical Fibers
Phase
The Factional Part of the Period of a Sinusoidal Wave, Usually Expressed in Electrical Degrees and Referenced to the origin
Core Hole Size
Physical Dimensions of the hole
Insertion Loss
The Loss in Load Power Due to the Insertion of a Component or Device at Some Point in a Transmission System
Dielectric Strength
Measure of the Electrical Strength of a Material as an Insulator, the Maximum Electrical Potential Gradient that a Material can withstand without Rupture, the Higher the Dielectric Strength of a Material the Better its Quality as an Insulator
Compatibility
Capability of Being Used with or Connected to Different Types of Devices or Components without any Modifications
Is Tamper-Resistant
Tamper resistance is resistance to tampering (intentional malfunction or sabotage) by either the normal users of a product, package, or system or others with physical access to it.
Connection
Between Discrete Points Allows the Flow of Electrons (Electric Current)
Connector
Refers to the specific types of connections a device uses to join electrical conductors and create an electrical circuit. When you select the first desired connector, a second filter will appear listing any connectors on the opposite end of your selected connector on a device.
Temperature Rating
The Designated / Rated / Maximum / Range Temperature at Which the Instrument May be Used in Continuous Operation without Loss of its Basic Properties and performance
Is Weather Resistant
Is this product listed as Weather Resistant ?
IP Rating
Levels of sealing effectiveness of electrical enclosures. IP20, IP55, IP53, IP68
Capacity
The Load for Which a Generating Unit, Generating Plant or Other Electrical Apparatus is Rated Either by the User or by the Manufacturer, Electrical Phenomenon Whereby an Electric Charge is Stored
Frequency Rating
The Number of Occurrences within a Given Time Period, the Rate at Which Alternating Current Makes a Complete Cycle of Reversals
Shape
The Type/Cross-Sectional Shape/Design/Geometric Shape/Physical Appearance of the item
Conductor Size
The Physical Dimension of Current Carrying Member of the Cable
Indoor/Outdoor
Enviromental Conditions rating on the product. Indoor Only, Outdoor, Both
Number of Ports
The Number of Application-Specific or Process-Specific Software Construct Serving as a Communication Endpoint / is Generally a Specific Place for Being Physically Connected to Some Other Device /A Number of Physical Access Point(S) Between a Conductor and
Input Voltage
The Difference of Electrical Potential Between Two Points of an Electrical or Electronic Circuit Entering a System
Number of Wires
The Number of Pliable Metallic Strand or Rod Made in Many Lengths and Diameters and are Electrically Insulated, Used Conduct Electricity
Bracket
The Type of Support, as of Metal or Wood, Projecting from a Wall or the Like to Hold or Bear the Weight of a Shelf, Part of a Cornice, Etc.
Availability
Product is available to buy on Legrand.us
Thickness
The Dimension Through an Object as Opposed to its Length or Width
Load Type
Denotes the type(s) of load that can be applied to a dimmer, which determines its compatible light sources.
Output Voltage
The Voltage Measured at the Output Terminals of a Power Supply
Overall Length
The Longest Dimension Measured from one End to Another End of the item
Number of Outlets
The Different Types of Receptacles Providing a Place in a Wiring System Where Current can be Taken to Supply Electrical Devices
Mounting Type
The way the item is mounted for display. The method by which a sign or label is affixed to a surface for display. Many signs will not have any defined mounting type and so will have no value captured for this attribute.
Number of Buttons
The Number of Keys/Switches in the item Used for Selecting a Particular Function
Number of Knockouts
How many knockouts are there in the product
Current Rating
Maximum Amount of Current a Cable can Carry Before Sustaining Damage or Deterioration
Number of Devices
The amount of devices the product can connect to.
Number of USBs
Number of USB ports
IP/Analog
Indicates Whether the System is analog or Network Connected
Maximum Wattage
Greatest Amount of Power in Watts
Number of Circuits
The Number of Networks that Has a Closed Loop, Giving a Return Path for the Current
Has Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Knockout Size
Physical dimension of the knock-out size, could be diameter or a range
Number of Holes
The Number of Hollows or Holes Provided in the item for Mounting/Fixing
Form Factor
The Size, Configuration, or Physical Arrangement of the Unit
Radius
The Minimum Radius one can Bend a Conduit to without Kinking it, Damaging it, or Shortening its Life
Rack Units Rack Units_030104
Unit Used to Describe the Height of Equipment Intended for Mounting
Enclosure Type
Style, Type, Size, Etc. of the Enclosure of a Device
Load Capacity
The Greatest Amount of Loading that a Instrument can Receive without Violating Quality Standards
Construction
The Act or Process of Constructing Which Includes Design and Manufacture Type
Handle Type
The Type/Shape of the Part that is Designed to be Held or Operated with the Hand
Number of Conductors
The Number of Materials/Strands/Pairs Which Contain Movable Electric Charges
Plating Specification
Describes the characteristics and standards of the metal plating used on a connector, which can impact the performance and reliability of signal transfer.
Shielded/Unshielded
Denotes whether a cable is designed with an extra layer of metal foil or braid surrounding the inner conductor to protect against electromagnetic interference (EMI).
Power Supply
The Specification of the Electrical Power or the Description of This Electrical Power Which is Required for the Proper Functioning of the item
Number of Channels
The Number of Media Used to Convey Information
Cord Length
The Linear Extent of Cord in Space from one End to the Other
Orientation
The Position or Alignment Relative to Points of the Compass or Other Specific Directions
Impedance
A Material's Opposition to the Flow of Electric Current
Simplex/Duplex
A Communications Network can Provide one-Way / Multi-Way Communication Service
NEMA Configuration Code
Alpha-Numeric Code Applied to Connectors to Guarantee Consistency and Interchageability Between Manufacturers
Load Rating
The maximum load that a device is designed to withstand without breakage or loss of performance.
Battery
A Device for Converting Chemical Energy Into Electrical Energy a Group of Two or More Connected Voltaic Cells
Response Time
The Time of System or Functional Unit Takes to React to a Given Input.
Wattage
amount of watts used
Connection TypeTooltip Title
Style or Type of Connection Used
Product Family
Used to identify and differentiate offerings within a particular product line. Product families are typically treated as adjectives. It is not recommended to use the product line (ex: Wiremold®) and product family names (Evolution™) together. This will introduce a level of unnecessary confusion for the audience.
Conduit Size
It is the Maximum Size of the Conduit
Conductor Range
The Size Range of the Metal Wires and Cables that Allow the Flow of Electrical Current
Maximum Product Height
The maximum measurable height of the product.
Conductor Material
The Material of Current Carrying Member of the Cable
Jaw Width
The Jaw Width of the Plier
Receptacle Type
The physical character of a Receptacle. The Type/Specification of a Contact Device Installed at the Outlet for the Connection of an Attachment Plug a Single Receptacle is a Single Contact Device with No Other Contact Device on the Same Yoke a Multiple Receptacle is Two or More Contact Devices.
Number of Types of Sources
To the Quantity and Type of Inputs for Instance, Hdmi, S-Video, Etc., Connections on a Device
Bottom Type
Bottom of Cable Tray
Fire Rating
The Period of Time a Building or Building Component Maintains the Ability to Confine a Fire or Continues to perform a Given Structural Function or Both, as Determined by Tests Prescribed in Section 703
Number of Switches
Number of electrical switches
Voltage
The Rate at Which Energy is Drawn from a Source that Produces a Flow of Electricity in a Circuit
Operating Temperature
The Temperature at Which the Unit is Safely Operated or Kept without Damaging or Changing the performance Characteristics of the Unit
Included
The Supplementary items Supplied with the Product Which May be Necessary for the Optimum Operation of the Product
Security
Protection of Information from theft or Corruption, or the Preservation of Availability
Supply Voltage
The Specified Amount and Type Voltage / Voltage Range for Which the Equipment is Rated for Operation
Product Has Potential to Contribute to LEED
This product contributes to earning credits in the LEED rating system.
Wire Connection Type
Describes the method used to connect wires to the device, such as screw terminals, push-in connectors, or lead wires.
Shield Type
Describes the internal safeguards (or lack of) built into a cable, connector, or port to protect against electromagnetic interference (EMI) and improve data retention.
Preset
Denotes whether a dimmer returns lights to their previously-selected light level when turned on.
Number of Pairs
Refers to the number of wire pairs a punch down block supports, which determines its capacity for handling voice or data circuits in networking installations.
Operating Temperature Min
Indicates the lowest possible temperature a device can be safely used without the risk of failure or damage.
Number of Connections
The number of connections a product is able to make to other devices.
Jacket Material
The outer material used to insulate a cord or cable's wiring.
Insulation Thickness
Describes the specific width of insulation material used by a device for electrical retention, signal conservation, general safety, etc.
Cable Diameter Range
The range of cable diameters that the grip can accommodate, ensuring a proper fit.
Battery Capacity
Describes the maximum amount of electrical charge that a battery can store and deliver.
Adapter Color
Indicates the specific color of the fiber adapter, which can be used to indicate the use or keyed type of the adapter.
Mesh Length
The overall length of a grip's mesh portion, which provides strength and protection to the cable.
Seismic Tested
Indicates whether a device has been tested to withstand and/or perform under certain seismic conditions.
Rack Depth
Refers to the depth of a rack that is usable to support rackmount equipment.
NEMA Load Class
Describes the official classification given to a product to indicate its effective load capacity, as defined by the National Electrical Manufacturers Association (NEMA). The designation can help determine the appropriate product based on the weight and volume of the cables it needs to support, ensuring safety and adherence to industry standards.
Screw Size
The physical dimensions, proportions, magnitude, or extent of a screw.
Eye Style
The design of the loop or eye at the end of a grip, used for attachment to hooks or other equipment.
Cutout Shape
The geometric form of the cutout area, which must match the shape of the device or component being installed.
Storage Temperature
Describes the temperature or range of temperatures at which a product can be safely stored or kept without damaging or altering the performance characteristics of the device.
Conductor Stranding
Indicates the configuration of wires used for electrical conduction. Solid conductors provide greater current capacity and increased durability, while stranded conductors provide greater flexibility.
USB Wattage
Describes the maximum electrical power a USB receptacle can safely output.
Cutout
Describes the available cutout styles on a product for either installing additional devices, or breaking and/or separating a portion of the circuit.
Maximum Insertion Loss
The maximum loss in load power due to the insertion of a component or device at some point in a transmission system.
Approximate Break Strength
The estimated force at which the mesh grip will fail, indicating the maximum load it can safely handle.
Termination Style
The style of connection used for electrical termination between two devices.
Ferrule
Denotes the material used in the fiber optic ferrule, which affects alignment precision, durability, and signal performance.
Frame
Describes characteristics of a device's frame that make it more suited for specific applications.
Fiber Size
The outer diameter of an optical fiber core, cladding and coating, expressing microns.
Wiring Configuration
Describes the specific internal wiring configuration of a device.
Dimming Compatibility
Describes the method(s) used by a device or system to adjust the brightness of a lighting load.
Working Load
The maximum load that can be routinely applied to a component in straight tension.
Polarity Type
The specific configuration used to map the "transmit" and "receive" fibers within a fiber optic system.
Fiber Optic Cable Type
The different types and characteristics of fiber optical cable designed for specific applications.
Wall Plate Included
Indicates if the device comes with a cover plate for aesthetic integration with the wall.
Minimum Floor Depth
The minimum depth a floor must be in order to properly install the product.
Works With
Need to ensure your choice works with your device, system, or software? Select your needs using this filter to confirm compatibility.
Tray Height
Refers to the approximate height of a cable tray used for specifying. Selecting a specific height will show cable trays with that height, as well as cable tray accessories compatible with that height.
Horsepower Rating
Refers to the power capacity of a device under normal load conditions, measured in horsepower (HP).
Capacitance
Describes the ability of two conductors to store electrical energy, which can impact a cable's signal propagation and delay.
Requires Neutral Wire
Indicates whether a device requires a neutral wire to function properly.
Mounting Hole Type
Describes the style of holes or openings used to either mount a device or mount to a device.
Form Size
Indicates the specific size or configuration of a device, often used to refer to the precise shape.
Connector Color
Refers to the color of a device's electrical or data connector.
Flanged
Indicates whether a device is designed with a raised edge/rim, on or around its receptacle, for superior strength, handling, or attachment to another object.
Receptacle Spacing
Refers to the distance between power outlets or receptacles on a device, which can be important for planning the layout of plugs and connectors.
Wall Plate Type
Refers to the style or intended usage of a wall plate.
Operating Humidity
Describes the range of humidity at which a device can be utilized safely without the risk of failure or damage.
Connection Location
Specifies where on the device the electrical connections are made, which can affect installation.
Jacket Application
Describes the specific application(s) a cable's jacket is designed to be used in, such as in-wall, plenum, or riser.
Jacket Color
Describes the color used on the outer covering of a cord or cable; often used as a way to easily identify different cables or signal types in networking setups.
Box Type
Describes any specific aspects or characteristics that may differentiate the box portion of a device.
Product Series
A collection of related products that share a common design, technology, or purpose. Products within the series either maintain a cohesive brand / style identity or work together to serve a particular solution.
NPT Thread Size
The size of the National Pipe Thread taper applied to fittings, indicating compatibility with American standard pipes.
Switch Type
Refers to the style or operation method used by a switch to control lighting or other electrical devices.
Box Capacity
Refers to the maximum number of gangs available within a box for installing electrical, networking, and/or AV devices and accessories.
Connectivity Footprint
Refers to the unique application or solution that products like connectivity adapters, jacks, or panels can fit within or are compatible with.
Wireless Range
Describes the maximum distance wireless devices can be separated while preserving signal quality and reliability.
Throw Type
Describes the method of switch operation, indicating whether it controls one circuit (single-throw) or switches between two circuits (double-throw).
Enclosure Size
The approximate height of the compatible wiring enclosure.
Service Capacity
Denotes the number of different services that can be used within a product as a result of separated internal compartments, including electrical, low voltage, water, air, and more.
Rung Spacing
Describes the distance between individual rungs in cable tray sections.
Mesh Type
The style or pattern of mesh used in a grip, which can affect the flexibility, strength, and type of strain relief provided.
Conductor
Describes the number and configuration of electrical wires used within a cable to transmit signals.
Grip Fitting
The type of fitting used to secure the grip to a cable, ensuring a firm hold and preventing damage to the cable.
Single/Multimode
Describes the mode of fiber either utilized or accepted by a device to transmit or receive a fiber optic signal.
Features
Unique characteristics and functionality that set the product apart from others in its field.
Bend Radius
The minimum radius a cable, cord, or wire can bend without kinking it, damaging it, or shortening its life.
Maximum Horsepower Rating
The maximum power load the device can handle before the risk of damage or failure.
Number of Phases
Indicates the number of electrical phases a device utilizes.
Number of Poles
Single pole switches have two terminals and control one light fixture from one location. 3-Way switches have three terminals and can control one fixture from two locations. 4-Way switches have four terminals can control one fixture from three locations. Multi-location refers to switches connected to a smart lighting system.
Internal Depth
Refers to the distance from the surface level of a box to the area where internal devices are plugged in, illustrating the available space within to accommodate cords, receptacles, and large devices.
Circular Outlet Diameter
Refers to the diameter of the circular opening in a wall plate, which should match the diameter of the outlet it is intended to cover.
Connects To
The types of devices and networks the devices is able to connect to.
Tray Width
Refers to the approximate width of a cable tray used for specifying. Selecting a specific width will show cable trays with that width, as well as cable tray accessories compatible with that width.
Operating Temperature Max
Indicates the highest possible temperature a device can be safely used without the risk of failure or damage.
Warranty Type
The product warranty that accompanies the specific product.
Typical Insertion Loss
Refers to the most common amount of signal lost at a connection/mating point, measured in decibels (dB).
Wall Plate Size
The general size of the the included wall plate. The size may determine whether it suits your personal application!
Terminal Accommodation
Describes the type and size of wire that the receptacle's terminals can securely hold (typically provided as a range in gauge size).
Cover Style
Refers to the style and design of cover used by the product for a specific application and/or aesthetic.
Environmental Conditions
Describes the relative range of climatic standards a device can safely operate within.
Finish
Describes the specific surface treatment applied to the outer product for either aesthetics and/or durability.
Wiring Location
Describes where incoming electrical connections can enter the enclosure, such as top, bottom, side, etc.
Cover Material
Refers to the material and/or finish used by the cover of the product.
Return Loss
Refers to the loss of power in the signal returned/reflected by a discontinuity in a transmission line or optical fiber.
Stud Size
The physical dimensions or proportions of the ring terminal or cable/wire lug.
Housing Color
Describes the color used for the outer housing on a device.
Performance Level/Tier
Describes the specific variation of performance capabilities a device is designed to support.
Maximum Power
Denotes the maximum electrical current that can be delivered by any given unit.
Jacket Rating
Denotes the NEC (National Electric Code) standards the outer casing/jacket surrounding a cable or cord's internal wiring and insulation is rated to.
Shuttered Adapters
Refers to to the cap/door mechanism on a panel or insert that remains closed to help prevent contaminants from entering the ferrule end face, but can be opened to insert/install a connector.
Connector Style
The design or type of the connector used to join electrical circuits together.
Depth Behind Device Plates
Refers to the distance between device plates within the product and the back of the product itself.
Outlet Type
Describes the unique qualities or characteristics of an electrical outlet that make it better suited to different uses. The listed qualities may give the outlet improved safety performance, increased efficiency, or additional functionality.
Installed Devices
Selection of devices that come pre-installed within a product.
Grip Angle
The angle at which a cable grip holds the cable, which can affect strain relief and the direction of cable entry.
Category Performance Application
Refers to the specific standard used to define an ethernet cable's capabilities and its intended usage. Most commonly shortened to"Cat" and a number (e.g. Cat5e; Cat6; Cat6a).
Material
Indicates the primary material(s) used to construct a product.
Wiring Method
Describes the design and ways of connecting various parts of a device with cable and/or wire.
Cable Diameter
The typical outer diameter of a cable.
USB Amperage
Describes the maximum electrical current the conductor or device can carry through its USB ports before sustaining immediate or progressive deterioration.
Application Sector
Refers to the expected environment(s) or intended usage(s) for a product (e.g. Residential, Commercial, Industrial, etc.).
Tray Length
Refers to the approximate length of a cable tray used for specifying. Selecting a specific length will show cable trays with that length.
Stock Level
Filter your results to only in-stock products sold directly on legrand.us.
Application Sector
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTrough Tee WHITE (4H, 20W)FTT100/500WH CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH VERT OUT 4x24 - BLACKFTVO90100/600BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH VERT IN COVER FOR 2x2 VERT IN - BLACKFTCVI9050/50BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH CABINET BRACKET 2H- BLACKFTCF50BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH VERT OUT COVER FOR 4x8 VERT OUT - BLACKFTCVO90100/200BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH HOLD DOWN - BLACK (2H)FTHDCL50BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTrough Blind End- PAINTED (4H,12W)FTBE100/300PE CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsVentilated Trough Straight(2H,2W, 120L) PAINTEDVT50/50PE CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH VERT OUT 2x12 - BLACKFTVO9050/300BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH 45 DEG BEND 2x2 - BLACKFTFB4550/50BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH TEE 2x12 - BLACKFTT50/300BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH 45 BEND COVER FOR 4'' WIDE 45 BEND - BLACKFTCFB45100BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH VERT OUT COVER FOR 4x4 VERT OUT - BLACKFTCVO90100/100BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH 90 Deg VERT OUT- PAINTED (4H, 8W)FTVO90100/200OR CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH 45 BEND COVER FOR 24'' WIDE 45 BEND - BLACKFTCFB45600BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsFiberTrough Cabinet Bracket-PAINTEDFTCF50PE CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTrough Blind End- PAINTED (4H,12W)FTBE50/100PE CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsVentilated Trough Straight (4H, 8W, 120L) PAINTEDVT100/200PE CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH 45 DEG BEND 2x12 - BLACKFTFB4550/300BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH VERT IN 2x4 - BLACKFTVI9050/100BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH VERT IN 4x8 - BLACKFTVI90100/200BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH 45 DEG BEND 4x12 - BLACKFTFB45100/300BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTROUGH VERT IN 4x4 - BLACKFTVI90100/100BL CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsFiberTrough Straight- PAINTED (4H,20W)FT100/500PE CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsVentilated Trough Straight(2H, 8W, 120L) PAINTEDVT50/200PE CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsVertical Fitting Divider5G-9112-99-S6 CablofilItray Aluminum cable tray provides superior support in long span industrial applications
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsFiberTrough 90 Bend Cvr- PAINTED (12W)FTCFB90300PE CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsTrough 90 Deg Bnd WHITE (2H, 8W)FTFB9050/200WH CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsFiberTrough 90 Bend Cvr- PAINTED (4W)FTCFB90100PE CablofilCablofil steel trough trays provide the strength and security required when then need to limit cable access is of primary importance.
-
Added to Favorites Go to favoritesRemove from favorites?Something went wrong. Please try again later.Product not added for comparison. Please remove any current selection to add this. Manage SelectionsWALL MOUNT ATTACHMENT-PAINTED (2D,2W,2L)C50PE CablofilCablofil wire mesh tray is the fastest most flexible and adaptable cable management system available